<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB circuit review needed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214298#M13386</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Dec 2012 10:43:33 GMT</pubDate>
    <dc:creator>teju</dc:creator>
    <dc:date>2012-12-26T10:43:33Z</dc:date>
    <item>
      <title>USB circuit review needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214296#M13384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I request a review of the USB circuits designed for the IMX.53. We intend using both the on chip USB's as hosts.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Teju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Dec 2012 11:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214296#M13384</guid>
      <dc:creator>teju</dc:creator>
      <dc:date>2012-12-20T11:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: USB circuit review needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214297#M13385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2012 05:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214297#M13385</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2012-12-26T05:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: USB circuit review needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214298#M13386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2012 10:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214298#M13386</guid>
      <dc:creator>teju</dc:creator>
      <dc:date>2012-12-26T10:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: USB circuit review needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214299#M13387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Teju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just one recommendation. When we use our channels as hosts, we use to place current limiters at VBUS just to make sure the USB max current specification is not exceeded. You can find examples of this in our reference designs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2013 18:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214299#M13387</guid>
      <dc:creator>JorgeRama_rezRi</dc:creator>
      <dc:date>2013-01-11T18:12:36Z</dc:date>
    </item>
    <item>
      <title>Re: USB circuit review needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214300#M13388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are running both as host ports, do you need to connect USB_OTG_VBUS and USB_H1_VBUS to +5V via an RC filter, or can it be left floating?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find the purpose of the VBUS pin in the literature. I'm assuming it is only used by the OTG port when it can operate as either an A or B port; to detect when external VBUS is applied. Is that correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2013 00:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-circuit-review-needed/m-p/214300#M13388</guid>
      <dc:creator>LeonCraven</dc:creator>
      <dc:date>2013-05-23T00:45:57Z</dc:date>
    </item>
  </channel>
</rss>