<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8QM Yocto Logo Rotation in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882680#M133802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on iMX8QM custom board with L4.14.78 Kernel BSP, in which yocto boot logo is coming up-side down (&lt;STRONG&gt;showing open-embedded as LOGO&lt;/STRONG&gt;) in MIPI-DSI LCD while booting kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to rotate that yocto boot logo to 180 degree.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way/command to change rotation/flip the yocto logo/image whle booting? &lt;BR /&gt;Kindly let me know the fix for logo rotation issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Prashanth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Feb 2019 08:26:39 GMT</pubDate>
    <dc:creator>prashanthkumar</dc:creator>
    <dc:date>2019-02-23T08:26:39Z</dc:date>
    <item>
      <title>iMX8QM Yocto Logo Rotation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882680#M133802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on iMX8QM custom board with L4.14.78 Kernel BSP, in which yocto boot logo is coming up-side down (&lt;STRONG&gt;showing open-embedded as LOGO&lt;/STRONG&gt;) in MIPI-DSI LCD while booting kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to rotate that yocto boot logo to 180 degree.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way/command to change rotation/flip the yocto logo/image whle booting? &lt;BR /&gt;Kindly let me know the fix for logo rotation issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Prashanth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Feb 2019 08:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882680#M133802</guid>
      <dc:creator>prashanthkumar</dc:creator>
      <dc:date>2019-02-23T08:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM Yocto Logo Rotation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882681#M133803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prashanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;preliminary patch were sent you via mail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Feb 2019 22:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882681#M133803</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-24T22:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM Yocto Logo Rotation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882682#M133804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need the patch, too. Can you send me the patch via mail?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2020 05:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882682#M133804</guid>
      <dc:creator>晓锋潘</dc:creator>
      <dc:date>2020-07-27T05:44:54Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM Yocto Logo Rotation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882683#M133805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can go to path&amp;nbsp;&lt;/P&gt;&lt;P&gt;sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-core/psplash/files/psplash-basic.service&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and change&lt;/P&gt;&lt;P&gt;[Service]&lt;BR /&gt;ExecStartPre=/bin/sh -c "if [ -e /sys/class/graphics/fbcon/cursor_blink ]; then echo 0 &amp;gt; /sys/class/graphics/fbcon/cursor_blink; fi"&lt;BR /&gt;ExecStart=/usr/bin/psplash --angle 90 -n&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;angle 90 is for 90 degree rotation, you may change as you wish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2020 11:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Yocto-Logo-Rotation/m-p/882683#M133805</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2020-07-27T11:37:38Z</dc:date>
    </item>
  </channel>
</rss>