<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ERROR: Function failed: do_compile (log file is located at /opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/temp/log.do_compile.112699)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882332#M133765</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="335895" data-username="yyuan@iraytek.com" href="https://community.nxp.com/people/yyuan@iraytek.com"&gt;袁 野&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the logs you have given I can see -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"To run this tool with Python 3.4 please install the 'typing' library with 'sudo pip3 install typing' or upgrade to Python 3.5+. If you don't have 'pip3' then you need to install it with 'sudo apt-get install python3-pip'"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check that are you using the correct python version as mentioned in the above comment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if the build is still failing after doing the mentioned changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Radhika Somaiya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Mar 2019 09:17:15 GMT</pubDate>
    <dc:creator>radhikasomaiya</dc:creator>
    <dc:date>2019-03-26T09:17:15Z</dc:date>
    <item>
      <title>ERROR: Function failed: do_compile (log file is located at /opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/temp/log.do_compile.112699)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882331#M133764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;UL style="color: #2e3033; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;&lt;LI style="margin: 0px 0px 10px;"&gt;&lt;P class="" data-group="1-1" style="color: #666666; font-size: 14px;"&gt;I have some compilation problems&lt;/P&gt;&lt;/LI&gt;&lt;LI style="margin: 0px 0px 10px;"&gt;when i do 'bitbake fsl-image-qt5-validation-imx -c populate_sdk',it is wrong.&lt;/LI&gt;&lt;LI style="margin: 0px 0px 10px;"&gt;DEBUG: Executing shell function do_compile&lt;BR /&gt;PlatformName: Yocto&lt;BR /&gt;WARNING: Environment variable FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR was not defined, so we force defined it.&lt;BR /&gt;Its highly recommended to manually define this variable so you can reuse the thirdparty libs between builds and repositories.&lt;BR /&gt;Read DocBuildingExternals.md for detailed information about this environment variable.&lt;BR /&gt;FSL_GRAPHICS_SDK=/opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git&lt;BR /&gt;FSL_GRAPHICS_SDK_ANDROID_PROJECT_DIR=/opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/Android&lt;BR /&gt;FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR=/opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty&lt;BR /&gt;ROOTFS=/opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot&lt;BR /&gt;To run this tool with Python 3.4 please install the 'typing' library with 'sudo pip3 install typing' or upgrade to Python 3.5+. If you dont have 'pip3' then you need to install it with 'sudo apt-get install python3-pip'&lt;BR /&gt;WARNING: exit code 1 from a shell command.&lt;BR /&gt;ERROR: Function failed: do_compile (log file is located at /opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/temp/log.do_compile.112699)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loading cache: 100% |#########################################################################################################################################################################| Time: 0:00:02&lt;BR /&gt;Loaded 3463 entries from dependency cache.&lt;BR /&gt;Parsing recipes: 100% |#######################################################################################################################################################################| Time: 0:00:23&lt;BR /&gt;Parsing of 2548 .bb files complete (2547 cached, 1 parsed). 3464 targets, 227 skipped, 7 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;BR /&gt;NOTE: Multiple providers are available for runtime ptpd (ptpd, ptpd-qoriq)&lt;BR /&gt;Consider defining a PREFERRED_RPROVIDER entry to match ptpd&lt;BR /&gt;NOTE: Multiple providers are available for runtime ptpd-dev (ptpd, ptpd-qoriq)&lt;BR /&gt;Consider defining a PREFERRED_RPROVIDER entry to match ptpd-dev&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.38.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-14.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6qsabresd"&lt;BR /&gt;DISTRO = "fsl-imx-x11"&lt;BR /&gt;DISTRO_VERSION = "4.14-sumo"&lt;BR /&gt;TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"&lt;BR /&gt;TARGET_FPU = "hard"&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:64a257fa22126c4a40ff7e03424a404e360ebe1e"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia = "HEAD:2bb21ef27c4b0c9d52d30b3b2c5a0160fd02b966"&lt;BR /&gt;meta-freescale = "HEAD:407c6cf408969445031a492e2d25e0e2749582ea"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:88a29631809d1af0df618245430db29f2a7012b5"&lt;BR /&gt;meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk = "HEAD:9867dae67c158e0820bf226bd18b792623e99b25"&lt;BR /&gt;meta-browser = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-python &lt;BR /&gt;meta-filesystems = "HEAD:2bb21ef27c4b0c9d52d30b3b2c5a0160fd02b966"&lt;BR /&gt;meta-qt5 = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"&lt;/P&gt;&lt;P&gt;WARNING: /opt/yocto/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.14.78.bb.do_compile is tainted from a forced run | ETA: 0:00:03&lt;BR /&gt;WARNING: /opt/yocto/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/imx-test/imx-test_git.bb.do_compile is tainted from a forced run&lt;BR /&gt;Initialising tasks: 100% |####################################################################################################################################################################| Time: 0:00:08&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;Currently 1 running tasks (6342 of 7832) 80% |############################################################################################################################## |&lt;BR /&gt;0: imx-gpu-sdk-5.2.0-r0 do_compile - 457s (pid 15185)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #666666; background-color: #ffffff; font-weight: normal; font-size: 14px;"&gt;I feel stuck.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #666666; background-color: #ffffff; font-weight: normal; font-size: 14px;"&gt;please help me!!!!!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #666666; background-color: #ffffff; font-weight: normal; font-size: 14px;"&gt;thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Mar 2019 02:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882331#M133764</guid>
      <dc:creator>yyuan</dc:creator>
      <dc:date>2019-03-23T02:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR: Function failed: do_compile (log file is located at /opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/temp/log.do_compile.112699)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882332#M133765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="335895" data-username="yyuan@iraytek.com" href="https://community.nxp.com/people/yyuan@iraytek.com"&gt;袁 野&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the logs you have given I can see -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"To run this tool with Python 3.4 please install the 'typing' library with 'sudo pip3 install typing' or upgrade to Python 3.5+. If you don't have 'pip3' then you need to install it with 'sudo apt-get install python3-pip'"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check that are you using the correct python version as mentioned in the above comment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if the build is still failing after doing the mentioned changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Radhika Somaiya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 09:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882332#M133765</guid>
      <dc:creator>radhikasomaiya</dc:creator>
      <dc:date>2019-03-26T09:17:15Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR: Function failed: do_compile (log file is located at /opt/yocto/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/temp/log.do_compile.112699)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882333#M133766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you ，&lt;/P&gt;&lt;P&gt;I changed a command and it worked，&lt;SPAN style="color: #666666; background-color: #ffffff; font-weight: normal; font-size: 14px;"&gt;I think that's ok&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2019 05:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-compile-log-file-is-located-at-opt/m-p/882333#M133766</guid>
      <dc:creator>yyuan</dc:creator>
      <dc:date>2019-03-27T05:32:54Z</dc:date>
    </item>
  </channel>
</rss>