<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6UL internal SNVS RTC counts too fast in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881520#M133637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the SNVS RTC with backup battery on imx6ul. I was able to enable it in kernel and device tree. From user space I can read it (hwclock -r) and set it to system time (hwclock -w). However, it runs way to fast, around +8 seconds faster per minute. This is more than 137ms per second. According to iMX6UL reference manual there is an RTC calibration register, however the maximum possible calibration value is&amp;nbsp;16/32768=488us per second, so no way I can compensate it this way. I know that internal clocks are quite inaccurate compared to external crystals, but I don't believe the difference is that big.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have an idea&amp;nbsp;what the problem could be?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2019 14:23:33 GMT</pubDate>
    <dc:creator>philippbachmann</dc:creator>
    <dc:date>2019-01-17T14:23:33Z</dc:date>
    <item>
      <title>i.MX6UL internal SNVS RTC counts too fast</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881520#M133637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the SNVS RTC with backup battery on imx6ul. I was able to enable it in kernel and device tree. From user space I can read it (hwclock -r) and set it to system time (hwclock -w). However, it runs way to fast, around +8 seconds faster per minute. This is more than 137ms per second. According to iMX6UL reference manual there is an RTC calibration register, however the maximum possible calibration value is&amp;nbsp;16/32768=488us per second, so no way I can compensate it this way. I know that internal clocks are quite inaccurate compared to external crystals, but I don't believe the difference is that big.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have an idea&amp;nbsp;what the problem could be?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 14:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881520#M133637</guid>
      <dc:creator>philippbachmann</dc:creator>
      <dc:date>2019-01-17T14:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL internal SNVS RTC counts too fast</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881521#M133638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Philipp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to Table 11. Oscillator and clock recommendations&lt;/P&gt;&lt;P&gt;Hardware Development Guide for the i.MX 6UltraLite Applications Processor&lt;/P&gt;&lt;P&gt;"..on-chip 40 kHz oscillator. The tolerance is ± 50%."&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fuser-guide%2FIMX6ULHDG.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 23:17:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881521#M133638</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-17T23:17:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL internal SNVS RTC counts too fast</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881522#M133639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did not expect that the tolerance is that big, thanks a lot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Philipp&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 09:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-internal-SNVS-RTC-counts-too-fast/m-p/881522#M133639</guid>
      <dc:creator>philippbachmann</dc:creator>
      <dc:date>2019-01-18T09:13:07Z</dc:date>
    </item>
  </channel>
</rss>