<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to do ack after receiving a CAN frame in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-do-ack-after-receiving-a-CAN-frame/m-p/881369#M133596</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dheeraj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;acknowledgement is described in sect.26.7.1 FLEXCAN Initialization Sequence&lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf" title="http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problems with transmit/receive CAN data frames may be in inproper can&lt;/P&gt;&lt;P&gt;line levels, one can check them with oscilloscope in both cases:&lt;/P&gt;&lt;P&gt;with analyzer and without it. Also one can check CAN_STBY signals&lt;/P&gt;&lt;P&gt;of can transceiver custom device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jan 2019 23:30:32 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-01-22T23:30:32Z</dc:date>
    <item>
      <title>How to do ack after receiving a CAN frame</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-do-ack-after-receiving-a-CAN-frame/m-p/881368#M133595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IMx 6ULL based design for my application, and configured CAN port for data frame reception. Unfortunatly I am not able to get the data from the bus(If the bus is occupied with transmitter and my device).&lt;/P&gt;&lt;P&gt;But if i introduce an CAN analyzer in the same bus my device will be able to receive CAN data frames.So my question is&lt;/P&gt;&lt;P&gt;1. Is the issue coming comming because of a inproper acknowledgement for received data? if that is the case how to rectify?&lt;/P&gt;&lt;P&gt;2. As per my understanding the acknowledgement must be handled in the physical layer not in Application layer, for this do I need to enable/set/disable any of the confihuration register,if so please do let me know the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dheeraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 10:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-do-ack-after-receiving-a-CAN-frame/m-p/881368#M133595</guid>
      <dc:creator>dheeraj_k</dc:creator>
      <dc:date>2019-01-17T10:46:36Z</dc:date>
    </item>
    <item>
      <title>Re: How to do ack after receiving a CAN frame</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-do-ack-after-receiving-a-CAN-frame/m-p/881369#M133596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dheeraj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;acknowledgement is described in sect.26.7.1 FLEXCAN Initialization Sequence&lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf" title="http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problems with transmit/receive CAN data frames may be in inproper can&lt;/P&gt;&lt;P&gt;line levels, one can check them with oscilloscope in both cases:&lt;/P&gt;&lt;P&gt;with analyzer and without it. Also one can check CAN_STBY signals&lt;/P&gt;&lt;P&gt;of can transceiver custom device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 23:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-do-ack-after-receiving-a-CAN-frame/m-p/881369#M133596</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-22T23:30:32Z</dc:date>
    </item>
  </channel>
</rss>