<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I cannot get IP assigned by DHCP nor nodejs latest version - imx6ulevk</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-cannot-get-nodejs-latest-version-imx6ulevk/m-p/881243#M133580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may add a layer to an image by adding following line to the conf/local.conf file inside the build directory, and then baking the image.&lt;BR /&gt;IMAGE_INSTALL_append = “ nodejs”&lt;BR /&gt; &lt;BR /&gt;Whenever you want to see which packages are available on the BSP you can run:&lt;BR /&gt;bitbake -s&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Apr 2019 03:48:46 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-04-05T03:48:46Z</dc:date>
    <item>
      <title>I cannot get nodejs latest version - imx6ulevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-cannot-get-nodejs-latest-version-imx6ulevk/m-p/881242#M133579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The repo approved by nxp in the Yocto manual documentation is not the latest one (master branch), but th rocko one. &lt;STRONG&gt;Why is this?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In OpenEmbedded Layer Index:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking rocko or master branch, it is only available version 7.10.0 for meta-nodejs (&lt;A class="link-titled" href="https://layers.openembedded.org/layerindex/branch/master/layer/meta-nodejs/" title="https://layers.openembedded.org/layerindex/branch/master/layer/meta-nodejs/"&gt;OpenEmbedded Layer Index - meta-nodejs&lt;/A&gt;&amp;nbsp;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In OpenEmbedded&amp;nbsp; Recipes Index:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;EM&gt;For rocko: v8.4.0&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;For master branch: v10.15.3&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, in recipes, there is no npm package and I need that too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, my questions are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Why the latest branch suggested by i.MX_Yocto_Project_User's_Guide is not the latest one? It repo sync brings rocko.&lt;/LI&gt;&lt;LI&gt;Should I repo sync the master? How do I do that?&lt;/LI&gt;&lt;LI&gt;How can I get latest npm as well? (v6.x.x) The layer meta-nodejs includes nodejs-npm as a package but it is not in the latest version.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 19:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-cannot-get-nodejs-latest-version-imx6ulevk/m-p/881242#M133579</guid>
      <dc:creator>gbassi1</dc:creator>
      <dc:date>2019-04-04T19:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot get IP assigned by DHCP nor nodejs latest version - imx6ulevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-cannot-get-nodejs-latest-version-imx6ulevk/m-p/881243#M133580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may add a layer to an image by adding following line to the conf/local.conf file inside the build directory, and then baking the image.&lt;BR /&gt;IMAGE_INSTALL_append = “ nodejs”&lt;BR /&gt; &lt;BR /&gt;Whenever you want to see which packages are available on the BSP you can run:&lt;BR /&gt;bitbake -s&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2019 03:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-cannot-get-nodejs-latest-version-imx6ulevk/m-p/881243#M133580</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-04-05T03:48:46Z</dc:date>
    </item>
  </channel>
</rss>