<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Which parameter to cross compile?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-parameter-to-cross-compile/m-p/881129#M133564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Paolo Santini,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a Hello World example on the following training:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95225"&gt;https://community.nxp.com/docs/DOC-95225&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also an example on this thread’s comments, which is a bit more up to date.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/394804"&gt;https://community.nxp.com/thread/394804&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Feb 2019 21:28:09 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-02-28T21:28:09Z</dc:date>
    <item>
      <title>Which parameter to cross compile?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-parameter-to-cross-compile/m-p/881128#M133563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I work on a SBC Variscite based on IMX6UL; to replace the second splashscreen I have to compile a .C file using "configure" command.&lt;/P&gt;&lt;P&gt;Some indications about how to cross compile from Linux ? My environment is:&lt;/P&gt;&lt;P&gt;/opt/fslc-x11/2.2.1/environment-setup-armv7at2hf-neon-fslc-linux-gnueabi&lt;/P&gt;&lt;P&gt;Some one could help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 17:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-parameter-to-cross-compile/m-p/881128#M133563</guid>
      <dc:creator>paolosantini</dc:creator>
      <dc:date>2019-02-21T17:30:12Z</dc:date>
    </item>
    <item>
      <title>Re: Which parameter to cross compile?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-parameter-to-cross-compile/m-p/881129#M133564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Paolo Santini,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a Hello World example on the following training:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95225"&gt;https://community.nxp.com/docs/DOC-95225&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also an example on this thread’s comments, which is a bit more up to date.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/394804"&gt;https://community.nxp.com/thread/394804&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2019 21:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-parameter-to-cross-compile/m-p/881129#M133564</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-02-28T21:28:09Z</dc:date>
    </item>
  </channel>
</rss>