<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Running kmscube as init</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881015#M133529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;You can since drm/kms is from linux kernel , not from weston&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need to change the framebuffer lib to hook up to frame buffer display. . export LD_PRELOAD=libVDK-framebuffer.so. libVDK.so is linked to libVDK-wayland.so by default.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just tried.&amp;nbsp; kmscube runs ok after killall weston and &lt;SPAN&gt;export LD_PRELOAD=libVDK-framebuffer.so&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;kmscube runs also without the export once weston is killed but Qt still doesn't, it needs an eglfs&amp;nbsp;QT_QPA_PLATFORM and changing the qtbase recipe&amp;nbsp;was not enough.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2019 15:34:00 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-02-12T15:34:00Z</dc:date>
    <item>
      <title>Running kmscube as init</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881014#M133528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I'm currently trying to optimize boottime of the IMX8MQ-EVK.&lt;/P&gt;&lt;P&gt;For this i wanted to use kmscube on a monitor connected with HDMI as an example application to replace init.&lt;/P&gt;&lt;P&gt;So far i have a bashscript which executes instead of init and launches kmscube (and after that init).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when kmscube should execute&amp;nbsp; it prints&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;could not open drm device&lt;BR /&gt;failed to initialize legacy DRM&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I tried to give it other devices from /dev/dri but with the same outcome.&lt;/P&gt;&lt;P&gt;So i thought about "attaching" the monitor before executing the script.&lt;/P&gt;&lt;P&gt;Unfortunately i have no idea how to do that.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2019 10:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881014#M133528</guid>
      <dc:creator>michael_kainz</dc:creator>
      <dc:date>2019-02-04T10:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: Running kmscube as init</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881015#M133529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;You can since drm/kms is from linux kernel , not from weston&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need to change the framebuffer lib to hook up to frame buffer display. . export LD_PRELOAD=libVDK-framebuffer.so. libVDK.so is linked to libVDK-wayland.so by default.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just tried.&amp;nbsp; kmscube runs ok after killall weston and &lt;SPAN&gt;export LD_PRELOAD=libVDK-framebuffer.so&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;kmscube runs also without the export once weston is killed but Qt still doesn't, it needs an eglfs&amp;nbsp;QT_QPA_PLATFORM and changing the qtbase recipe&amp;nbsp;was not enough.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 15:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881015#M133529</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-02-12T15:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: Running kmscube as init</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881016#M133530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer!&lt;BR /&gt;I used the core-image-minimal and didn't add libvdk-imx at first. So weston isn't even included in the image.&lt;/P&gt;&lt;P&gt;Now that does solve the issue i submitted but it still doesn't work.&lt;/P&gt;&lt;P&gt;It seems like kmscube gets interrupted or cant work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any more ideas?&lt;/P&gt;&lt;P&gt;Here is the script:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;#!/bin/sh&lt;/P&gt;&lt;P&gt;echo "Starting needed programm"&lt;BR /&gt;export LD_PRELOAD=libVDK-framebuffer.so&lt;BR /&gt;export QT_QPA_PLATFORM=eglfs&lt;BR /&gt;exec /usr/bin/kmscube -D /dev/dri/card0 &amp;amp;&lt;BR /&gt;exec /sbin/init&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Here is the bootlog. At "&lt;SPAN style="background-color: #f6f6f6;"&gt;Starting needed programm" my script gets called.&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+g0b5c4c8bf2 (Feb 05 2019 - 10:47:53 +0100)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX8MQ rev2.0 1500 MHz (running at 1000 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 26C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX8MQ EVK&lt;BR /&gt;DRAM: 3 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110]&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;No panel detected: default to HDMI&lt;BR /&gt;Display: HDMI (1280x720)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt; - ATF 6a83ae0&lt;BR /&gt; - U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+g0b5c4c8bf2&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;Net: eth0: ethernet@30be0000&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;reading boot.scr&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;reading Image&lt;BR /&gt;20335104 bytes read in 447 ms (43.4 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;reading fsl-imx8mq-evk.dtb&lt;BR /&gt;42111 bytes read in 17 ms (2.4 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt; Booting using the fdt blob at 0x43000000&lt;BR /&gt; Using Device Tree in place at 0000000043000000, end 000000004300d47e&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0&lt;BR /&gt;[ 0.000000] Linux version 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d61147 (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #5 SMP PREEMPT Thu Jan 31 14:31:44 CET 2019&lt;BR /&gt;[ 0.000000] Boot CPU: AArch64 Processor [410fd034]&lt;BR /&gt;[ 0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030860000 (options '115200')&lt;BR /&gt;[ 0.000000] bootconsole [ec_imx6q0] enabled&lt;BR /&gt;[ 0.302962] dmi: Firmware registration failed.&lt;BR /&gt;[ 1.152133] NXP PHY: loading NXP PHY driver: [autonomous mode]&lt;BR /&gt;[ 1.174831] Can't support &amp;gt; 32 bit dma.&lt;BR /&gt;[ 1.265917] ov5640_read_reg:write reg error:reg=300a&lt;BR /&gt;[ 1.374396] Can't support &amp;gt; 32 bit dma.&lt;BR /&gt;[ 1.380814] Can't support &amp;gt; 32 bit dma.&lt;BR /&gt;[ 1.385754] Failed to run desc RNG4 SH0 status (0xfffffff5)&lt;BR /&gt;[ 1.391504] Failed to run desc RNG4 SH1 status (0xfffffff5)&lt;BR /&gt;[ 1.532655] Can't support &amp;gt; 32 bit dma.&lt;BR /&gt;[ 1.537435] Can't support &amp;gt; 32 bit dma.&lt;BR /&gt;[ 1.565159] caam-snvs 30370000.caam-snvs: can't get snvs clock&lt;BR /&gt;[ 1.585229] ak5558 1-0013: ak5558_i2c_probe(748)&lt;BR /&gt;[ 1.616743] wm8524-codec wm8524: Supported sample rate: 192000Hz&lt;BR /&gt;[ 1.622786] wm8524-codec wm8524: Supported sample rate: 96000Hz&lt;BR /&gt;[ 1.628779] wm8524-codec wm8524: Supported sample rate: 48000Hz&lt;BR /&gt;[ 1.634713] wm8524-codec wm8524: Supported sample rate: 32000Hz&lt;BR /&gt;[ 1.654687] ak4458 1-0010: ASoC: failed to probe component -6&lt;BR /&gt;[ 1.660491] imx-ak4458 sound-ak4458: ASoC: failed to instantiate card -6&lt;BR /&gt;[ 1.667325] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-6)&lt;BR /&gt;[ 1.689701] ak5558 1-0013: ASoC: failed to probe component -6&lt;BR /&gt;[ 1.695540] imx-ak5558 sound-ak5558: ASoC: failed to instantiate card -6&lt;BR /&gt;[ 1.702308] imx-ak5558 sound-ak5558: snd_soc_register_card failed (-6)&lt;BR /&gt;[ 1.801716] imx-pcie 33800000.pcie: Speed change timeout&lt;BR /&gt;[ 2.063679] imx-pcie 33c00000.pcie: phy link never came up&lt;BR /&gt;[ 2.069192] imx-pcie 33c00000.pcie: failed to initialize host&lt;BR /&gt;[ 2.074946] imx-pcie 33c00000.pcie: unable to add pcie port.&lt;BR /&gt;Starting needed programm&lt;BR /&gt;[ 1] Failed to open device: No such file or directory, Try again...&lt;BR /&gt;Using display 0x3baa06b0 with EGL version 1.5&lt;BR /&gt;===================================&lt;BR /&gt;EGL information:&lt;BR /&gt; version: "1.5"&lt;BR /&gt; vendor: "Vivante Corporation"&lt;BR /&gt; client extensions: "EGL_EXT_client_extensions EGL_EXT_platform_base EGL_KHR_platform_wayland EGL_EXT_platform_wayland EGL_KHR_platform_gbm"&lt;BR /&gt; display extensions: "EGL_KHR_fence_sync EGL_KHR_reusable_sync EGL_KHR_wait_sync EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbuffer_image EGL_EXT_image_dma_buf_import EGL_KHR_lock_surface EGL_KHR_create_context EGL_KHR_surfaceless_context EGL_EXT_create_context_robustness EGL_EXT_protected_surface EGL_EXT_protected_content EGL_EXT_buffer_age EGL_WL_bind_wayland_display EGL_WL_create_wayland_buffer_from_image EGL_KHR_partial_update EGL_EXT_image_dma_buf_import_modifiers"&lt;BR /&gt;===================================&lt;BR /&gt;OpenGL ES 2.x information:&lt;BR /&gt; version: "OpenGL ES 3.1 V6.2.4.p1.150331"&lt;BR /&gt; shading language version: "OpenGL ES GLSL ES 3.10"&lt;BR /&gt; vendor: "Vivante Corporation"&lt;BR /&gt; renderer: "Vivante GC7000L"&lt;BR /&gt; extensions: "GL_OES_vertex_type_10_10_10_2 GL_OES_vertex_half_float GL_OES_element_index_uint GL_OES_mapbuffer GL_OES_vertex_array_object GL_OES_compressed_ETC1_RGB8_texture GL_OES_compressed_paletted_texture GL_OES_texture_npot GL_OES_rgb8_rgba8 GL_OES_depth_texture GL_OES_depth_texture_cube_map GL_OES_depth24 GL_OES_depth32 GL_OES_packed_depth_stencil GL_OES_fbo_render_mipmap GL_OES_get_program_binary GL_OES_fragment_precision_high GL_OES_standard_derivatives GL_OES_EGL_image GL_OES_EGL_sync GL_OES_texture_stencil8 GL_OES_shader_image_atomic GL_OES_texture_storage_multisample_2d_array GL_OES_required_internalformat GL_OES_surfaceless_context GL_OES_copy_image GL_OES_draw_buffers_indexed GL_OES_texture_border_clamp GL_OES_texture_buffer GL_OES_texture_cube_map_array GL_OES_draw_elements_base_vertex GL_OES_texture_half_float GL_OES_texture_float GL_KHR_blend_equation_advanced GL_KHR_debug GL_KHR_robustness GL_KHR_robust_buffer_access_behavior GL_EXT_texture_type_2_10_10_10_REV GL_EXT_texture_filter_anisotropic GL_EXT_texture_compression_dxt1 GL_EXT_texture_format_BGRA8888 GL_EXT_texture_compression_s3tc GL_EXT_read_format_bgra GL_EXT_multi_draw_arrays GL_EXT_frag_depth GL_EXT_discard_framebuffer GL_EXT_blend_minmax GL_EXT_multisampled_render_to_texture GL_EXT_color_buffer_half_float GL_EXT_color_buffer_float GL_EXT_robustness GL_EXT_texture_sRGB_decode GL_EXT_draw_buffers_indexed GL_EXT_texture_border_clamp GL_EXT_texture_buffer GL_EXT_copy_image GL_EXT_texture_cube_map_array GL_EXT_multi_draw_indirect GL_EXT_draw_elements_base_vertex GL_EXT_texture_rg GL_EXT_protected_textures GL_EXT_sRGB GL_VIV_direct_texture "&lt;BR /&gt;===================================&lt;BR /&gt;user interrupted!&lt;BR /&gt;failed to queue page flip: Device or resource busy&lt;BR /&gt;[ 3.864238] ol_download_firmware: chip_id:0x5030000 board_id:0x0&lt;BR /&gt;[ 4.265382] __ol_transfer_bin_file: Failed to get athsetup.bin:-11&lt;BR /&gt;[ 4.890172] __wmi_control_rx : event handler is not registered: event id 0x1d019&lt;/P&gt;&lt;P&gt;NXP i.MX Release Distro 4.9.88-2.0.0 imx8mqevk ttymxc0&lt;/P&gt;&lt;P&gt;imx8mqevk login:&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 13:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-kmscube-as-init/m-p/881016#M133530</guid>
      <dc:creator>michael_kainz</dc:creator>
      <dc:date>2019-02-15T13:18:29Z</dc:date>
    </item>
  </channel>
</rss>