<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX25 pixel clock</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152043#M1335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;vga=330 in kernel command line fixed this..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 May 2012 05:12:37 GMT</pubDate>
    <dc:creator>Venku</dc:creator>
    <dc:date>2012-05-03T05:12:37Z</dc:date>
    <item>
      <title>iMX25 pixel clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152041#M1333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use an optrex 3.5" LCD with the foll spec:&lt;/P&gt;&lt;P&gt;refresh rate: 50&lt;BR /&gt; x – resolution: 320&lt;BR /&gt; y –resolution: 240&lt;BR /&gt; pixel clock: 9.8MHz&lt;BR /&gt; left_margin: Horizontal back porch: 68&lt;BR /&gt; right_margin: Horizontal front porch: 20&lt;BR /&gt; upper_margin: Vertical back porch: 2&lt;BR /&gt; lower_margin: Vertical front porch: 2&lt;BR /&gt; hsync_len: HSYNC width: 30&lt;BR /&gt; vsync_len: VSYNC width: 11&lt;BR /&gt; sync; (VERTICAL / HORIZONTAL SYNC HIGH ACTIVE): VERTICAL / HORIZONTAL SYNC Active Low&lt;BR /&gt; vmode; (NON INTERLACED/ INTERLACED / ODD / DOUBLE): NON INTERLACED&lt;/P&gt;&lt;P&gt;The following changes were made to mxc_modedb.c:&lt;/P&gt;&lt;P&gt;"LCD_OPTREX", 50, 320, 240, 102040, 68, 20, 2, 2, 30, 11,&lt;BR /&gt; /*FB_SYNC_OE_LOW_ACT,*/&lt;BR /&gt; FB_SYNC_CLK_LAT_FALL,&lt;BR /&gt; FB_VMODE_NONINTERLACED,&lt;BR /&gt; 0,},&lt;/P&gt;&lt;P&gt;where LCD_OPTREX would be the name i have assigned.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; Everything works fine (display, apps show up, TS), except that I don't get the splash screen (kernel boot logo)!&lt;/P&gt;&lt;P&gt;The 102040 value was arrived at by doing a KHZ2PICO(9800) {9.8MHz pixel clock}. Is this wrong?&lt;/P&gt;&lt;P&gt;Observations:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Apr 2012 05:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152041#M1333</guid>
      <dc:creator>Venku</dc:creator>
      <dc:date>2012-04-07T05:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX25 pixel clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152042#M1334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried the calculation from Jacky's post too:&lt;/P&gt;&lt;P&gt;&lt;A href="http://imxcommunity.org/profiles/blogs/linux-framebuffer-driver-calculate-pixel-clock-for-struct-fb" target="_blank"&gt;http://imxcommunity.org/profiles/blogs/linux-framebuffer-driver-calculate-pixel-clock-for-struct-fb&lt;/A&gt;&lt;/P&gt;&lt;P&gt;which puts a value of 179067. But no luck :(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Venkat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Apr 2012 06:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152042#M1334</guid>
      <dc:creator>Venku</dc:creator>
      <dc:date>2012-04-07T06:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX25 pixel clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152043#M1335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;vga=330 in kernel command line fixed this..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2012 05:12:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX25-pixel-clock/m-p/152043#M1335</guid>
      <dc:creator>Venku</dc:creator>
      <dc:date>2012-05-03T05:12:37Z</dc:date>
    </item>
  </channel>
</rss>