<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8 Gstreamer Pipelines in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879959#M133424</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I send the command for camera transcode to you for reference:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;gst-launch-1.0 v4l2src ! video/x-raw,format=NV12,width=1920,height=1080 ! queue max-size-time=0 ! vpuenc_h264 ! h264parse ! vpudec ! queue max-size-time=0 ! waylandsink enable-tile=true sync=false&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;you can change the parameter you want,like width ,height, format&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Mar 2019 03:07:32 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2019-03-26T03:07:32Z</dc:date>
    <item>
      <title>i.MX8 Gstreamer Pipelines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879956#M133421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was curious if at any point there may be a listing of gstreamer pipeline examples for the i.MX8.&amp;nbsp; Something similar to this thread for the i.MX6 &lt;A href="https://community.nxp.com/docs/DOC-93387"&gt;https://community.nxp.com/docs/DOC-93387&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I have been doing some development between the SW encoder in the i.MX 8M and the HW encoder in the i.MX 8M Mini.&amp;nbsp; I have gstreamer pipelines working for video streaming from the CSIMIPI camera to the HDMI port and files.&amp;nbsp; I also have a working pipeline for the SW encoder on the i.MX 8M. I am in need of an example of a pipeline that will encode the camera CSIMIPI camera at 1920 x 1080 to a fakesink or file for the i.MX 8M Mini.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 23:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879956#M133421</guid>
      <dc:creator>shawnnageli</dc:creator>
      <dc:date>2019-03-08T23:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Gstreamer Pipelines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879957#M133422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.mx8M don't have encoding HW, for SW encoding, pls refer to the link as below:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/476358?commentID=1029609#comment-1029609" title="https://community.nxp.com/thread/476358?commentID=1029609#comment-1029609"&gt;https://community.nxp.com/thread/476358?commentID=1029609#comment-1029609&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 06:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879957#M133422</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-03-21T06:29:08Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Gstreamer Pipelines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879958#M133423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I am aware the i.MX 8M does not have a hardware encoder.&amp;nbsp; I have the software encoder working for the i.MX 8M but wanted to do HW encoding with the&lt;STRONG&gt; i.MX 8M Mini&lt;/STRONG&gt; (Which has a hardware encoder) for a comparison and was inquiring regarding gstreamer commands to do that with the &lt;STRONG&gt;i.MX 8M Mini&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2019 15:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879958#M133423</guid>
      <dc:creator>shawnnageli</dc:creator>
      <dc:date>2019-03-22T15:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Gstreamer Pipelines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879959#M133424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I send the command for camera transcode to you for reference:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;gst-launch-1.0 v4l2src ! video/x-raw,format=NV12,width=1920,height=1080 ! queue max-size-time=0 ! vpuenc_h264 ! h264parse ! vpudec ! queue max-size-time=0 ! waylandsink enable-tile=true sync=false&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;you can change the parameter you want,like width ,height, format&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 03:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Gstreamer-Pipelines/m-p/879959#M133424</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-03-26T03:07:32Z</dc:date>
    </item>
  </channel>
</rss>