<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Keep repeating starting kernel.... in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879242#M133318</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Possibly the kernel fails because of some memory failure.&lt;BR /&gt;Please try to perform memory test:&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also please try to remove as many devices from the configuration as possible.&lt;BR /&gt;There is a chance that some driver is wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Feb 2019 07:24:25 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-02-22T07:24:25Z</dc:date>
    <item>
      <title>Keep repeating starting kernel....</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879241#M133317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using imx6 Dual Lite with 1G and take Android6.0 as my OS system.&lt;/P&gt;&lt;P&gt;I'm having an issue with repeating starting kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I burned my image in, I repower the machine and the debug log shows as below.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.04 (Feb 15 2019 - 13:37:19)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6DL rev1.3 at 792 MHz&lt;BR /&gt;CPU: Temperature 40 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;forenex victor board_init!&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;No panel detected: default to AUO_G185XW01&lt;BR /&gt;forenex victor enable lvds!&lt;BR /&gt;forenex victor backlight = 0&lt;BR /&gt;forenex victor backlight again = 0&lt;BR /&gt;forenex victor LVDS pwm = 0&lt;BR /&gt;Display: AUO_G185XW01 (1366x768)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;forenex victor board_late_init!&lt;BR /&gt;forenex victor backlight = 0&lt;BR /&gt;check_and_clean: reg 0, flag_set 0&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;boota mmc2&lt;BR /&gt;kernel @ 14008000 (8593408)&lt;BR /&gt;ramdisk @ 15000000 (1028493)&lt;BR /&gt;fdt @ 14f00000 (39172)&lt;BR /&gt;## Booting Android Image at 0x12000000 ...&lt;BR /&gt;Kernel load addr 0x14008000 size 8392 KiB&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=FX100 cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled&lt;BR /&gt;## Flattened Device Tree blob at 14f00000&lt;BR /&gt; Booting using the fdt blob at 0x14f00000&lt;BR /&gt; Loading Kernel Image ... OK&lt;BR /&gt; Using Device Tree in place at 14f00000, end 14f0c903&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.04 (Feb 15 2019 - 13:37:19)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6DL rev1.3 at 792 MHz&lt;BR /&gt;CPU: Temperature 43 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;forenex victor board_init!&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;No panel detected: default to AUO_G185XW01&lt;BR /&gt;forenex victor enable lvds!&lt;BR /&gt;forenex victor backlight = 0&lt;BR /&gt;forenex victor backlight again = 0&lt;BR /&gt;forenex victor LVDS pwm = 0&lt;BR /&gt;Display: AUO_G185XW01 (1366x768)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;forenex victor board_late_init!&lt;BR /&gt;forenex victor backlight = 0&lt;BR /&gt;check_and_clean: reg 0, flag_set 0&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;boota mmc2&lt;BR /&gt;kernel @ 14008000 (8593408)&lt;BR /&gt;ramdisk @ 15000000 (1028493)&lt;BR /&gt;fdt @ 14f00000 (39172)&lt;BR /&gt;## Booting Android Image at 0x12000000 ...&lt;BR /&gt;Kernel load addr 0x14008000 size 8392 KiB&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=FX100 cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled&lt;BR /&gt;## Flattened Device Tree blob at 14f00000&lt;BR /&gt; Booting using the fdt blob at 0x14f00000&lt;BR /&gt; Loading Kernel Image ... OK&lt;BR /&gt; Using Device Tree in place at 14f00000, end 14f0c903&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.04 (Feb 15 2019 - 13:37:19)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6DL rev1.3 at 792 MHz&lt;BR /&gt;CPU: Temperature 43 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;forenex victor board_init!&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;No panel detected: default to AUO_G185XW01&lt;BR /&gt;forenex victor enable lvds!&lt;BR /&gt;forenex victor backlight = 0&lt;BR /&gt;forenex victor backlight again = 0&lt;BR /&gt;forenex victor LVDS pwm = 0&lt;BR /&gt;Display: AUO_G185XW01 (1366x768)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;forenex victor board_late_init!&lt;BR /&gt;forenex victor backlight = 0&lt;BR /&gt;check_and_clean: reg 0, flag_set 0&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;boota mmc2&lt;BR /&gt;kernel @ 14008000 (8593408)&lt;BR /&gt;ramdisk @ 15000000 (1028493)&lt;BR /&gt;fdt @ 14f00000 (39172)&lt;BR /&gt;## Booting Android Image at 0x12000000 ...&lt;BR /&gt;Kernel load addr 0x14008000 size 8392 KiB&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=FX100 cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled&lt;BR /&gt;## Flattened Device Tree blob at 14f00000&lt;BR /&gt; Booting using the fdt blob at 0x14f00000&lt;BR /&gt; Loading Kernel Image ... OK&lt;BR /&gt; Using Device Tree in place at 14f00000, end 14f0c903&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;It keeps repeating Starting kernel... over and over again.&lt;/P&gt;&lt;P&gt;How can I solve this problem????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 08:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879241#M133317</guid>
      <dc:creator>wangtsungli</dc:creator>
      <dc:date>2019-02-21T08:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: Keep repeating starting kernel....</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879242#M133318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Possibly the kernel fails because of some memory failure.&lt;BR /&gt;Please try to perform memory test:&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also please try to remove as many devices from the configuration as possible.&lt;BR /&gt;There is a chance that some driver is wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2019 07:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879242#M133318</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-02-22T07:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: Keep repeating starting kernel....</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879243#M133319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;A _jive_internal="true" data-id="287445" data-objecttype="3" data-orig-content="tsung li wang" data-type="person" href="https://community.nxp.com/people/wangtsungli"&gt;tsung li wang&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try these &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX6_M6.0.1_2.1.0_AN_DEMO_SD_BSP&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null&amp;amp;lang_cd=en"&gt;prebuilt images&lt;/A&gt; of i.MX6DL/6Q/6QP in your board. As I am able to boot the board using these images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shivani Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2019 11:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879243#M133319</guid>
      <dc:creator>shivanipatel</dc:creator>
      <dc:date>2019-02-22T11:32:00Z</dc:date>
    </item>
    <item>
      <title>Re: Keep repeating starting kernel....</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879244#M133320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/shivanipatel"&gt;shivanipatel&lt;/A&gt;‌ Thanks for your reply.&lt;/P&gt;&lt;P&gt;I have found the problem.&lt;/P&gt;&lt;P&gt;It's because of DTS settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 07:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-repeating-starting-kernel/m-p/879244#M133320</guid>
      <dc:creator>wangtsungli</dc:creator>
      <dc:date>2019-03-14T07:01:59Z</dc:date>
    </item>
  </channel>
</rss>