<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Linux hangs if UART is stressed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878667#M133253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miguel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with nxp releases from &lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx" title="https://source.codeaurora.org/external/imx/linux-imx"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or better with latest linux L4.14.78&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.11_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.11_1.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can try to disable uart sdma and use polling option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2019 01:17:11 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-01-17T01:17:11Z</dc:date>
    <item>
      <title>Linux hangs if UART is stressed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878666#M133252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a custom board which sports an iMX6 SOLO running Yocto with Kernel version 4.9.11-02307-gb200f6d.&lt;BR /&gt; My application uses serial communication with RS485 transceiver attached to the serial comms.&lt;BR /&gt;Pin control configuration -DTS- and UART initialization&amp;nbsp;are described below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no problem with such configuration when frame length sent through the serial ports is below 20-30 bytes but when frame length is above these values, eventually -sometimes it takes some minutes- the whole system hangs -by 'hangs' I meant that system gets unresponsive and I can't even connect through SSH, needing to restart Linux-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A simple while(1) sending a single byte causes this problem within seconds.&lt;BR /&gt; The problem is not related to one specific UART as it happens on other 3&amp;nbsp;UARTs configured the same way.&lt;BR /&gt; If I insert a delay when sending those bytes the problem never happens but obviously, this is not a satisfactory solution.&lt;/P&gt;&lt;P&gt;Is there something that I'm missing that could cause this issue?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;DTS configuration:&lt;/P&gt;&lt;PRE class="language-javascript line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;uart2 &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;names &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"default"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl&lt;SPAN class="number token"&gt;-0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;pinctrl_uart2_3&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;uart&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;has&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;rtscts&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; status &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"okay"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

pinctrl_uart2_3&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; uart2grp&lt;SPAN class="number token"&gt;-3&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;pins &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6QDL_PAD_EIM_D27__UART2_RX_DATA&amp;nbsp;&amp;nbsp; &lt;SPAN class="number token"&gt;0x1b0b1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6QDL_PAD_EIM_D26__UART2_TX_DATA&amp;nbsp;&amp;nbsp; &lt;SPAN class="number token"&gt;0x1b0b1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6QDL_PAD_EIM_D28__UART2_CTS_B&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="number token"&gt;0x1b0b1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART&amp;nbsp;inicialization:&lt;/P&gt;&lt;PRE class="language-cpp line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; rs485 &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;::&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;open&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"/dev/ttymxc1"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rs485&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; serial_rs485 rs485conf&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; rs485conf&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;flags &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; rs485conf&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;flags &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SER_RS485_ENABLED&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; rs485conf&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;flags &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SER_RS485_RTS_ON_SEND&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ioctl &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;rs485&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; TIOCSRS485&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;rs485conf&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;qDebug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;QString&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"Error writing ioctl port (%1): %2"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;arg&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;errno&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;arg&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;strerror&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;errno&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; &lt;SPAN class="token boolean"&gt;false&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; 
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;UART stress -running in a separate thread-:&lt;/P&gt;&lt;PRE class="language-cpp line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; byte &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xff&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;writeData&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;byte&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 09:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878666#M133252</guid>
      <dc:creator>miguelhortelano</dc:creator>
      <dc:date>2019-01-16T09:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Linux hangs if UART is stressed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878667#M133253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miguel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with nxp releases from &lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx" title="https://source.codeaurora.org/external/imx/linux-imx"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or better with latest linux L4.14.78&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.11_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.11_1.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can try to disable uart sdma and use polling option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 01:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878667#M133253</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-17T01:17:11Z</dc:date>
    </item>
    <item>
      <title>Re: Linux hangs if UART is stressed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878668#M133254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thks Igor.&lt;/P&gt;&lt;P&gt;I followed your last suggestion and disabled DMA for both Tx/Rx in DTS files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-javascript line-numbers"&gt;&lt;CODE&gt;uart2&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; serial@&lt;SPAN class="number token"&gt;021e8000&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"fsl,imx6q-uart"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"fsl,imx21-uart"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; reg &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x021e8000&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x4000&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupts &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;27&lt;/SPAN&gt; IRQ_TYPE_LEVEL_HIGH&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; clocks &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;clks IMX6QDL_CLK_UART_IPG&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;clks IMX6QDL_CLK_UART_SERIAL&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; clock&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;names &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"ipg"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"per"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/*dmas = &amp;lt;&amp;amp;sdma 27 4 0&amp;gt;, &amp;lt;&amp;amp;sdma 28 4 0&amp;gt;;
&amp;nbsp;&amp;nbsp;&amp;nbsp; dma-names = "rx", "tx";*/&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; status &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="string token"&gt;"disabled"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;This way solves the issue and now the system never hangs. Also this change increases the UART performance for short frames length -we usually transmit blocks with less than&amp;nbsp;32 bytes which is below the Tx FIFO length-.&lt;/P&gt;&lt;P&gt;I'll dig into this problem to find out why&amp;nbsp;UART's DMA could cause such behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 08:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-hangs-if-UART-is-stressed/m-p/878668#M133254</guid>
      <dc:creator>miguelhortelano</dc:creator>
      <dc:date>2019-01-17T08:34:34Z</dc:date>
    </item>
  </channel>
</rss>