<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックdevregs problems ... Error reading CPU type</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878147#M133221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a IMX6ULLEVK board with installed devregs&lt;/P&gt;&lt;P&gt;Calling devregs I see:&lt;/P&gt;&lt;P&gt;Error reading CPU type&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my /proc/cpuinfo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor : 0&lt;BR /&gt;model name : ARMv7 Processor rev 5 (v7l)&lt;BR /&gt;BogoMIPS : 3.00&lt;BR /&gt;Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae &lt;BR /&gt;CPU implementer : 0x41&lt;BR /&gt;CPU architecture: 7&lt;BR /&gt;CPU variant : 0x0&lt;BR /&gt;CPU part : 0xc07&lt;BR /&gt;CPU revision : 5&lt;/P&gt;&lt;P&gt;Hardware : Freescale i.MX6 UltraLite (Device Tree)&lt;BR /&gt;Revision : 0000&lt;BR /&gt;Serial : 0000000000000000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Apr 2019 15:25:45 GMT</pubDate>
    <dc:creator>fabio_poiatti</dc:creator>
    <dc:date>2019-04-03T15:25:45Z</dc:date>
    <item>
      <title>devregs problems ... Error reading CPU type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878147#M133221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a IMX6ULLEVK board with installed devregs&lt;/P&gt;&lt;P&gt;Calling devregs I see:&lt;/P&gt;&lt;P&gt;Error reading CPU type&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my /proc/cpuinfo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor : 0&lt;BR /&gt;model name : ARMv7 Processor rev 5 (v7l)&lt;BR /&gt;BogoMIPS : 3.00&lt;BR /&gt;Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae &lt;BR /&gt;CPU implementer : 0x41&lt;BR /&gt;CPU architecture: 7&lt;BR /&gt;CPU variant : 0x0&lt;BR /&gt;CPU part : 0xc07&lt;BR /&gt;CPU revision : 5&lt;/P&gt;&lt;P&gt;Hardware : Freescale i.MX6 UltraLite (Device Tree)&lt;BR /&gt;Revision : 0000&lt;BR /&gt;Serial : 0000000000000000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2019 15:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878147#M133221</guid>
      <dc:creator>fabio_poiatti</dc:creator>
      <dc:date>2019-04-03T15:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: devregs problems ... Error reading CPU type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878148#M133222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems there is no&amp;nbsp; .dat files for that processor, one can check answer on&lt;/P&gt;&lt;P&gt;similar issue on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/357410"&gt;devregs support for 6sololite&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/imx-utils/blob/master/devregs.cpp" title="https://github.com/boundarydevices/imx-utils/blob/master/devregs.cpp"&gt;imx-utils/devregs.cpp at master · boundarydevices/imx-utils · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2019 23:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878148#M133222</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-04-03T23:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: devregs problems ... Error reading CPU type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878149#M133223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Error CPU type seem to be related to Revision equal 0 ...and -c option to set from the shell the cpu name is not working&lt;/P&gt;&lt;P&gt;giving the error&amp;nbsp;&lt;/P&gt;&lt;P&gt;"unknown option c"&lt;/P&gt;&lt;P&gt;In addiction, the file /proc/cpuinfo I'm not able to modify setting a different revision&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 11:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devregs-problems-Error-reading-CPU-type/m-p/878149#M133223</guid>
      <dc:creator>fabio_poiatti</dc:creator>
      <dc:date>2019-04-04T11:40:59Z</dc:date>
    </item>
  </channel>
</rss>