<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mq CPU Temperature in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877816#M133196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="222397" data-username="bineyamtafesse" href="https://community.nxp.com/people/bineyamtafesse"&gt;bineyam&lt;/A&gt;，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For i.mx8MQ application, the better choice is to use a &lt;SPAN&gt;heatsink&lt;/SPAN&gt; according to real application.&lt;/P&gt;&lt;P&gt;In addition, The limit temperature of die is 125 degrees Celsius.&amp;nbsp; So, you can't configure the temperature to exceed 125 degrees Celsius.&amp;nbsp; Probably 115 degrees Celsius can meet your requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;NXP TIC team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Apr 2019 08:12:33 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2019-04-17T08:12:33Z</dc:date>
    <item>
      <title>imx8mq CPU Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877815#M133195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running the following configuratoin&lt;BR /&gt;CPU: imx8mq (custom PCB)&lt;/P&gt;&lt;P&gt;Linux OS: Linux 4.9.123&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed the TMU generated temperature exceeded warnings and cutoff on power up. The critical temperature limit of 95C was tripped (the processors were nowhere near this temperature). I modified the trip-temperature to 125C and the device boots through u-boot and kernel and functions as intended (and has been working for weeks).&amp;nbsp; Now, increasing the temperature is a temporary solution.&amp;nbsp; What is the expectation in terms of calibration? I see there is a definition in the u-boot under "tmu" that looks like a calibration table.&amp;nbsp; Is the expectation that we calibrate every unit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2019 21:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877815#M133195</guid>
      <dc:creator>bineyamtafesse</dc:creator>
      <dc:date>2019-04-03T21:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq CPU Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877816#M133196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="222397" data-username="bineyamtafesse" href="https://community.nxp.com/people/bineyamtafesse"&gt;bineyam&lt;/A&gt;，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For i.mx8MQ application, the better choice is to use a &lt;SPAN&gt;heatsink&lt;/SPAN&gt; according to real application.&lt;/P&gt;&lt;P&gt;In addition, The limit temperature of die is 125 degrees Celsius.&amp;nbsp; So, you can't configure the temperature to exceed 125 degrees Celsius.&amp;nbsp; Probably 115 degrees Celsius can meet your requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;NXP TIC team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 08:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877816#M133196</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2019-04-17T08:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq CPU Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877817#M133197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/weidong.sun"&gt;weidong.sun&lt;/A&gt;‌,&lt;BR /&gt;&lt;BR /&gt;The issue is that on immediate power-on (from room temperature), the u-boot reads 112 Celsius. Clearly, the chip is not heating up to 112C&amp;nbsp; in less than 10 seconds while only pulling 2W.&amp;nbsp; This is why I'm asking if additional calibration is needed.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 20:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/877817#M133197</guid>
      <dc:creator>bineyamtafesse</dc:creator>
      <dc:date>2019-04-19T20:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq CPU Temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/1291700#M175452</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/16474"&gt;@bineyamtafesse&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My IMX8M custom board has the&amp;nbsp;similar issue, Have you fixed the issue or not ?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 01:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-CPU-Temperature/m-p/1291700#M175452</guid>
      <dc:creator>jming</dc:creator>
      <dc:date>2021-06-14T01:58:57Z</dc:date>
    </item>
  </channel>
</rss>