<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: TCP Network performace issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TCP-Network-performace-issues/m-p/876396#M133025</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to use iperf2 instead of iperf3. There are some issues with iperf3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also please note that i.MX series are more multimedia than networking processors.&lt;BR /&gt;It is not optimized for top Ethernet speed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jan 2019 08:48:15 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-01-29T08:48:15Z</dc:date>
    <item>
      <title>TCP Network performace issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TCP-Network-performace-issues/m-p/876395#M133024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm evaluating the i.MX 8M processor to be used in a new project. Therefore i'm using the i.MX 8M Quad Evaluation Kit with the most recent prebuild embedded linux image 4.14.78.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A key feature for me is the TCP network performance throughput and response time.&lt;/P&gt;&lt;P&gt;My setup is a point to point connection between the eval board and a Win 7 PC with dedicated network interface Intel PRO/1000 PT.&lt;/P&gt;&lt;P&gt;Out of the box i've hard trouble to reach the expected gigabit performance or echo response times.&lt;/P&gt;&lt;P&gt;For measurement i've been using the iperf3 (v3.1.3) and also a simple python stupid script wich uses sockets.&lt;/P&gt;&lt;P&gt;The maximum of transfer speed i can achieve is about:&lt;/P&gt;&lt;P&gt;PC --&amp;gt; i.MX 8M =&amp;nbsp;360 MBit/s&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;i.MX 8M --&amp;gt; PC =&amp;nbsp;570 MBit/s&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Echo Response = 1.2 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The Echo Response is measured with the python script sending 64 Byte and receives this again. Also the quiet common ping command show this slow response for &amp;gt; 1ms in comparison to others with &amp;lt; 1ms.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For comparison i've used a Avnet UltraZ SOM evaluation board with equal setup and can achieve the expected performance:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;PC --&amp;gt;&amp;nbsp;UltraZ = 800 MBit/s&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;UltraZ&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;--&amp;gt; PC =&lt;SPAN&gt;&amp;nbsp;900&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;MBit/s&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Echo Response = 75&amp;nbsp;us&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can anyone confirm this performance issues and possibly explain that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any hardware bottleneck or is it more driver/software issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your support&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Vinzennz&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 07:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TCP-Network-performace-issues/m-p/876395#M133024</guid>
      <dc:creator>sevi</dc:creator>
      <dc:date>2019-01-16T07:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: TCP Network performace issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TCP-Network-performace-issues/m-p/876396#M133025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to use iperf2 instead of iperf3. There are some issues with iperf3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also please note that i.MX series are more multimedia than networking processors.&lt;BR /&gt;It is not optimized for top Ethernet speed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 08:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TCP-Network-performace-issues/m-p/876396#M133025</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-01-29T08:48:15Z</dc:date>
    </item>
  </channel>
</rss>