<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Help with Boot Mode Configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-Boot-Mode-Configuration/m-p/875947#M132990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having an issue with Boot mode configuration.&amp;nbsp; &amp;nbsp;I tie Boot_mode_1 to ground and tie Boot_mode_0 to 3V via 4.9k resistor, and the IMX6 Dual/Quad processor still looks at port pins to set configuration - DDR memory configuration is set to the wrong state because I use a pull-up on EIM_A20.&amp;nbsp; I thought Boot_mode_1 had to be high for this to occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if I ground both Boot_mode_0 and Boot_mode_1, my USB does not function even though EMMC has not received programming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2019 16:04:50 GMT</pubDate>
    <dc:creator>james_carter</dc:creator>
    <dc:date>2019-01-15T16:04:50Z</dc:date>
    <item>
      <title>Help with Boot Mode Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-Boot-Mode-Configuration/m-p/875947#M132990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having an issue with Boot mode configuration.&amp;nbsp; &amp;nbsp;I tie Boot_mode_1 to ground and tie Boot_mode_0 to 3V via 4.9k resistor, and the IMX6 Dual/Quad processor still looks at port pins to set configuration - DDR memory configuration is set to the wrong state because I use a pull-up on EIM_A20.&amp;nbsp; I thought Boot_mode_1 had to be high for this to occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if I ground both Boot_mode_0 and Boot_mode_1, my USB does not function even though EMMC has not received programming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 16:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-Boot-Mode-Configuration/m-p/875947#M132990</guid>
      <dc:creator>james_carter</dc:creator>
      <dc:date>2019-01-15T16:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: Help with Boot Mode Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-Boot-Mode-Configuration/m-p/875948#M132991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach jtag and check SRC_SBMR1,2 registers, described in&lt;BR /&gt;sect.60.7.2 SRC Boot Mode Register 1 (SRC_SBMR1).&lt;/P&gt;&lt;P&gt;Reason for wrong boot reading may be hardware, unstable clocks (24MHz, 32.768KHz crystals),&amp;nbsp;&lt;/P&gt;&lt;P&gt;power supplies ripples, one can check board using i.MX6 System Development User’s Guide&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fuser-guide%2FIMX6DQ6SDLHDG.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Check if clocks are stable when POR was released, just for test one can try to prolong&lt;BR /&gt;POR up to 1.sec.&lt;/P&gt;&lt;P&gt;May be recommended to look on i.MX6Sabre SD schematic and compare it with custom board:&lt;/P&gt;&lt;P&gt;Schematics (1)&lt;BR /&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Fsabre-development-system%2Fsabre-platform-for-smart-devices-based-on-the-i.mx-6-series%3ARDIMX6SABREPLAT%3Ffpsp%3D1%26tab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 23:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-Boot-Mode-Configuration/m-p/875948#M132991</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-15T23:32:47Z</dc:date>
    </item>
  </channel>
</rss>