<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: About create image from emmc using mfgtool/usb-otg</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-create-image-from-emmc-using-mfgtool-usb-otg/m-p/875881#M132983</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mingyang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for emmc programming one can follow Linux Guide from nxp linux documentation:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null" title="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null"&gt;https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or tutorial from&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/programming-emmc-on-i-mx6/" title="https://boundarydevices.com/programming-emmc-on-i-mx6/"&gt;Programming eMMC on i.MX6 - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2019 02:57:28 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-01-17T02:57:28Z</dc:date>
    <item>
      <title>About create image from emmc using mfgtool/usb-otg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-create-image-from-emmc-using-mfgtool-usb-otg/m-p/875880#M132982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I want to create a factory image from my board. The board only have emmc. I use mfgtool to burn image to emmc.And now i want to get image from /dev/mmcblk1p1. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Now i'm writing the image to u-disk via usb-otg. But the system is running while i use 'dd' command to get image from /dev/mmcblk1p1.If some files changes while creating images, the images will go wrong.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; So can i use mfgtool get image from board? Or just mount emmc to pc as a disk via usb-otg?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 10:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-create-image-from-emmc-using-mfgtool-usb-otg/m-p/875880#M132982</guid>
      <dc:creator>cyndent</dc:creator>
      <dc:date>2019-01-16T10:59:19Z</dc:date>
    </item>
    <item>
      <title>Re: About create image from emmc using mfgtool/usb-otg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-create-image-from-emmc-using-mfgtool-usb-otg/m-p/875881#M132983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mingyang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for emmc programming one can follow Linux Guide from nxp linux documentation:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null" title="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null"&gt;https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or tutorial from&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/programming-emmc-on-i-mx6/" title="https://boundarydevices.com/programming-emmc-on-i-mx6/"&gt;Programming eMMC on i.MX6 - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 02:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-create-image-from-emmc-using-mfgtool-usb-otg/m-p/875881#M132983</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-17T02:57:28Z</dc:date>
    </item>
  </channel>
</rss>