<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6ULL internal Flash jtag programming</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-internal-Flash-jtag-programming/m-p/875638#M132931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karsten&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for programming images to flash MFG Tool is used, this is described in&lt;/P&gt;&lt;P&gt;sect.5 Run a demo using Manufacturing Tool (MFGTool)&lt;/P&gt;&lt;P&gt;Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives&lt;/P&gt;&lt;P&gt;For nand one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-236994"&gt;How-To use NAND boot on i.MX6UL EVK board&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately I am not aware of options for programming flashes using jtag.&lt;/P&gt;&lt;P&gt;i.MX6ULL has not internal flash-memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Feb 2019 00:01:58 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-02-01T00:01:58Z</dc:date>
    <item>
      <title>i.MX6ULL internal Flash jtag programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-internal-Flash-jtag-programming/m-p/875637#M132930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;at the moment I am starting with the i.MX6ULL at a custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the document "Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives " to nice start.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Until now I was able to download and debug (Segger Base Debug Probe) the "Hello World"&amp;nbsp; example from SDK_2.2_MCIM6ULL .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded in the DDR and it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I would like to download and debug in the flash memory. Is this possible with an internal flash-memory of the i.MX6 or&amp;nbsp; is it necessary to have an external flash-memory ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In&amp;nbsp; the memory map is a QSPI1 Memory, is this only for external connection or is this a real internal flash which i can use to program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="memory_map_iMX6ULL.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64047i232F181347B7CEAB/image-size/large?v=v2&amp;amp;px=999" role="button" title="memory_map_iMX6ULL.PNG" alt="memory_map_iMX6ULL.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Moreover I have an external NAND Flash. Is it possible to program this via Jtag and use it for my application ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Karsten&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 13:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-internal-Flash-jtag-programming/m-p/875637#M132930</guid>
      <dc:creator>karsten</dc:creator>
      <dc:date>2019-01-31T13:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ULL internal Flash jtag programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-internal-Flash-jtag-programming/m-p/875638#M132931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karsten&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for programming images to flash MFG Tool is used, this is described in&lt;/P&gt;&lt;P&gt;sect.5 Run a demo using Manufacturing Tool (MFGTool)&lt;/P&gt;&lt;P&gt;Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives&lt;/P&gt;&lt;P&gt;For nand one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-236994"&gt;How-To use NAND boot on i.MX6UL EVK board&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately I am not aware of options for programming flashes using jtag.&lt;/P&gt;&lt;P&gt;i.MX6ULL has not internal flash-memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 00:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-internal-Flash-jtag-programming/m-p/875638#M132931</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-01T00:01:58Z</dc:date>
    </item>
  </channel>
</rss>