<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Memory Allocation and Estimation in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874310#M132747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the input. This will be helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2019 12:25:34 GMT</pubDate>
    <dc:creator>rvalvekar</dc:creator>
    <dc:date>2019-02-12T12:25:34Z</dc:date>
    <item>
      <title>Memory Allocation and Estimation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874308#M132745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello fellow NXP Users and Developers,&lt;/P&gt;&lt;P&gt;I have been researching into using i.MX Processors for Video Processing application and had few doubts about Memory Planning and Estimation.&lt;/P&gt;&lt;P&gt;Since it is hard to determine the exact pin point memory requirement of any application which involves a bit of researching for custom hardware and software, it is Hard to plan out the Memory Estimation using the development boards.&lt;/P&gt;&lt;P&gt;With respect to Graphical Processing especially with Image Processing and Camera Systems, Memory is the most important part of the system.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been searching the forum for a Memory Planning and Estimation discussion, but have not go a satisfactory answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well I would like to know and get to know better, and understand better with a academic perspective, that how can we do a memory estimation with imx processors which Must have the functionality of GPU and VPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Most of the high end development boards have 4 GB RAM, on which most of the things do work efficiently. But what i want to know is what is the minimum threshold for memory when it comes to GPU and VPU based applications.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there any golden mean for memory estimations with GPU and VPU applications ?&lt;/LI&gt;&lt;LI&gt;Does the memory estimation involves sharing of memory ? So the memory is shared between a GPU and the CPU ?&lt;/LI&gt;&lt;LI&gt;Can we have a dedicated memory just for GPU and VPU ?&lt;/LI&gt;&lt;LI&gt;Are there any other ways, like non conventional ways to have a memory estimation ?&lt;/LI&gt;&lt;LI&gt;How to make sure that the memory planning is also thought about with respect to power consumption&lt;/LI&gt;&lt;LI&gt;Is it possible to load the memory and activate it, but not use it ? So for example if I have 2 GB of memory, then basically 2 GB will be initialized, but 1 GB will be used. When there is need of extra memory, the buffer memory can be used, something like SMART Memory.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any other thoughts would be most welcome.&lt;/P&gt;&lt;P&gt;Thank You and appreciate the much help and support needed with memory estimation.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rohan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 12:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874308#M132745</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-01-30T12:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Allocation and Estimation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874309#M132746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rohan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;may be useful to check below documents&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/445874"&gt;How many GPU memory used in Linux 3.10.53?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/307038"&gt;Memory Reserved on i.MX6 for VPU&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100482"&gt;A Deep Dive into Image Processing for i.MX 6 Series Applications Processors&lt;/A&gt;&lt;A href="https://community.nxp.com/docs/DOC-93591"&gt;https://community.nxp.com/docs/DOC-93591&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am afraid there is no way to calculate it exactly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Feb 2019 00:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874309#M132746</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-02T00:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Allocation and Estimation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874310#M132747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the input. This will be helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 12:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Memory-Allocation-and-Estimation/m-p/874310#M132747</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-02-12T12:25:34Z</dc:date>
    </item>
  </channel>
</rss>