<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to create new image include changes. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-create-new-image-include-changes/m-p/874189#M132736</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kyumin Park,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mfg-tool image inherits from the mfgtool-initramfs-image.bbclass, which depends on the linux-mfgtool package for the kernel which sets the kernel as “mfgtool”.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that you would need to change the defconfig for linux-imx-mfgtool. The recipe is the same kernel recipe with the configuration provided by this defconfig.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Feb 2019 21:44:05 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-02-28T21:44:05Z</dc:date>
    <item>
      <title>How to create new image include changes.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-create-new-image-include-changes/m-p/874188#M132735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I have i.MX8QM board and build the image&amp;nbsp;using bitbake command .&lt;/P&gt;&lt;P&gt;I modified kernel driver and&amp;nbsp;make kernel. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd like to make&amp;nbsp;build image for&amp;nbsp;mfg-tool download.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to create new mfg-tool image include modified kernel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 10:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-create-new-image-include-changes/m-p/874188#M132735</guid>
      <dc:creator>kyumini0702</dc:creator>
      <dc:date>2019-02-19T10:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to create new image include changes.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-create-new-image-include-changes/m-p/874189#M132736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kyumin Park,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mfg-tool image inherits from the mfgtool-initramfs-image.bbclass, which depends on the linux-mfgtool package for the kernel which sets the kernel as “mfgtool”.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that you would need to change the defconfig for linux-imx-mfgtool. The recipe is the same kernel recipe with the configuration provided by this defconfig.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2019 21:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-create-new-image-include-changes/m-p/874189#M132736</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-02-28T21:44:05Z</dc:date>
    </item>
  </channel>
</rss>