<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mfgtool : Waiting for /dev/utp to appear</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873776#M132686</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Latest L4.14.78 uses uuu instead mfg tool. Please, see the below guide of how to use the uuu tool. It says that is for the i.MX8, but all the i.MX6 families are supported.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-341877"&gt;i.MX 8 Universal Update Utility (UUU) Tools and Pins Tool&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2019 22:38:19 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2019-02-19T22:38:19Z</dc:date>
    <item>
      <title>mfgtool : Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873775#M132685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem with my board imx6sxsabresd and BSP&amp;nbsp;imx-yocto-L4.14.78_1.0.0_ga.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i use ramfs provided in mfgtool package (L4.9.88_2.0.0_mfg-tool) i can program my sabresd board.&lt;/P&gt;&lt;P&gt;I compile mfgtool firmwares and it seems that my ramfs is not well builded.&lt;/P&gt;&lt;P&gt;Changing fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot by the files builded with Yocto, mfgtool stuck at this line :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freeing unused kernel memory: 1024K&lt;BR /&gt;Found New UDC: ci_hdrc.0&lt;BR /&gt;ci_hdrc.0 0&lt;BR /&gt;ffs.utp0&lt;BR /&gt;file system registered&lt;BR /&gt;Mass Storage Function, version: 2009/09/11&lt;BR /&gt;LUN: removable file: (no medium)&lt;BR /&gt;run utp at /dev/usb-utp0/ep0&lt;BR /&gt;.&lt;BR /&gt;uuu fastboot client 1.0.0 [built read descriptors&lt;BR /&gt;Feb 1 2019 12:47:25]&lt;BR /&gt;Start initread strings&lt;BR /&gt; usb&lt;BR /&gt;write string&lt;BR /&gt;&lt;STRONG&gt;Start handle command&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;uuc /dev/utp&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;uuc 0.5 [built Feb 1 2019 12:47:25]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;UTP: Waiting for /dev/utp to appear&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;configfs-gadget gadget: high-speed config #1: c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me ?&lt;/P&gt;&lt;P&gt;Today i can program my sabresd board with prebuild ramfs but with my futur custom boards, it will not be possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 11:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873775#M132685</guid>
      <dc:creator>florian_germain</dc:creator>
      <dc:date>2019-02-19T11:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool : Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873776#M132686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Latest L4.14.78 uses uuu instead mfg tool. Please, see the below guide of how to use the uuu tool. It says that is for the i.MX8, but all the i.MX6 families are supported.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-341877"&gt;i.MX 8 Universal Update Utility (UUU) Tools and Pins Tool&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 22:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873776#M132686</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2019-02-19T22:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool : Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873777#M132687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Yocto Sumo version.&lt;/P&gt;&lt;P&gt;The kernel boots up on yocto setup but there is no /dev/utp device node in the rootfs.&lt;/P&gt;&lt;P&gt;1. what kernel configuration need to be done inorder to create "/dev/utp" at boot up?&lt;/P&gt;&lt;P&gt;2. Also what is the major minor numbers of /dev/utp device node.&lt;/P&gt;&lt;P&gt;i am trying "uuc /dev/utp" which is not working.&lt;/P&gt;&lt;P&gt;3. Also the MFG tool on windows gets disconnected on kernel boot up on the yocto setup.&lt;/P&gt;&lt;P&gt;Is this expected behavior before launching uuc /dev/utp?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Anush D.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#MFG&lt;/P&gt;&lt;P&gt;#FSL_UTP&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2020 12:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-Waiting-for-dev-utp-to-appear/m-p/873777#M132687</guid>
      <dc:creator>anush_deekonda</dc:creator>
      <dc:date>2020-06-30T12:21:47Z</dc:date>
    </item>
  </channel>
</rss>