<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Accessing CAN Issue in IMX6ULL- evk yocto    in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873695#M132662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please let me know if there is any solution for the same&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for advance&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Mar 2019 09:48:01 GMT</pubDate>
    <dc:creator>bipulpandey</dc:creator>
    <dc:date>2019-03-12T09:48:01Z</dc:date>
    <item>
      <title>Accessing CAN Issue in IMX6ULL- evk yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873692#M132659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having an issue&amp;nbsp;to accessing CAN in our hardware while building the yocto image for imx6ul7d. when I used the prebuilt image of imxul7d(rocko) I am able to access CAN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver is enumerated and I am able to find in ip link&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx6ul7d:~# ip link&lt;/STRONG&gt;&lt;BR /&gt;1: lo: &amp;lt;LOOPBACK,UP,LOWER_UP&amp;gt; mtu 65536 qdisc noqueue qlen 1&lt;BR /&gt;link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00&lt;BR /&gt;2: &lt;STRONG&gt;can0: &amp;lt;NOARP40000&amp;gt; mtu 16 qdisc noop qlen 10&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;link/[280]&lt;/STRONG&gt;&lt;BR /&gt;3: can1: &amp;lt;NOARP40000&amp;gt; mtu 16 qdisc noop qlen 10&lt;BR /&gt;link/[280]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I tried to set the IP, I get an error&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx6ul7d:~# ip link set can0 up type can bitrate 125000&lt;BR /&gt;ip&lt;STRONG&gt;: either "dev" is duplicate, or "type" is garbage&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;However, I am able to set the bitrate prebuilt image.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the summery&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. take the prebuilt the image imx6ul7d able to communicate&amp;nbsp;through CAN&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Setup the environment fro yocto&amp;nbsp;follow the document&amp;nbsp; "i.MX_Yocto_Project_User's_Guide"&amp;nbsp; for imx6uul evk.&lt;/P&gt;&lt;P&gt;3. check all the component of CAN and iproute2 and found everything is fine.&lt;/P&gt;&lt;P&gt;4. checked with rocko, sumo,&amp;nbsp;thud but same issue.&lt;/P&gt;&lt;P&gt;5. I am taken all the documentation form imx6uulevk&amp;nbsp;&lt;/P&gt;&lt;P&gt;6. I have checked with imx6ull evk and imx6ul7d but same result.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what needs to be changed so that I can set bitrate&amp;nbsp;&lt;/P&gt;&lt;P&gt;what is this issue so we are getting&amp;nbsp;&lt;STRONG&gt;NOARP40000&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 09:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873692#M132659</guid>
      <dc:creator>bipulpandey</dc:creator>
      <dc:date>2019-02-19T09:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing CAN Issue in IMX6ULL- evk yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873693#M132660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi bipul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do not know the Mx6ul7d but I have worked with FlexCAN; If you do the next:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ip -s -d link show can0&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should get more info about the CAN module state, like if either is in error active or passive mode.&lt;/P&gt;&lt;P&gt;may be useful to check&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="1437" data-objecttype="102" href="https://community.nxp.com/docs/DOC-1437"&gt;All Boards FlexCAN&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also one can try with "canutils" package&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Flinux-can%2Fcan-utils%2Fblob%2Fmaster%2FREADME.md" rel="nofollow" target="_blank"&gt;can-utils/README.md at master · linux-can/can-utils · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 21:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873693#M132660</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-02-19T21:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing CAN Issue in IMX6ULL- evk yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873694#M132661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am getting this output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6ul7d:~# ip -s -d link show can0&lt;BR /&gt;BusyBox v1.24.1 (2019-02-18 19:05:54 UTC) multi-call binary.&lt;/P&gt;&lt;P&gt;Usage: ip [OPTIONS] {address | route | link | tunnel | } {COMMAND}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Though I am having Flexcan only&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have an entry in net&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx6ul7d:/# cd sys/class/net/&lt;BR /&gt;root@imx6ul7d:/sys/class/net# ls&lt;BR /&gt;can0 can1 eth0 eth1 lo sit0&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;the busy box&amp;nbsp;version V1.24.1&lt;/P&gt;&lt;P&gt;As I have mentioned we can communicate with CAN when I used a prebuilt image&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 09:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873694#M132661</guid>
      <dc:creator>bipulpandey</dc:creator>
      <dc:date>2019-02-20T09:12:07Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing CAN Issue in IMX6ULL- evk yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873695#M132662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please let me know if there is any solution for the same&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for advance&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 09:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/873695#M132662</guid>
      <dc:creator>bipulpandey</dc:creator>
      <dc:date>2019-03-12T09:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing CAN Issue in IMX6ULL- evk yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/1313765#M177511</link>
      <description>&lt;P&gt;Similar issue encountered.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 08:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-CAN-Issue-in-IMX6ULL-evk-yocto/m-p/1313765#M177511</guid>
      <dc:creator>adamhuang</dc:creator>
      <dc:date>2021-07-27T08:48:34Z</dc:date>
    </item>
  </channel>
</rss>