<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SCFW debug using Lauterbach JTAG</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873030#M132621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can trace M4 core of i.MX8 processor with Lauterbach as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jan 2019 05:26:56 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-01-16T05:26:56Z</dc:date>
    <item>
      <title>SCFW debug using Lauterbach JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873029#M132620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to debug system controller firmware on imx8qxpmek using lauterbach JTAG debugger?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 05:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873029#M132620</guid>
      <dc:creator>vmuthusu</dc:creator>
      <dc:date>2019-01-14T05:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW debug using Lauterbach JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873030#M132621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can trace M4 core of i.MX8 processor with Lauterbach as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 05:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873030#M132621</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-01-16T05:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW debug using Lauterbach JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873031#M132622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor&lt;/P&gt;&lt;P&gt;Thanks for your reply. I tried to load the scfw_tcm.elf using the data.load.elf command. After loading the PC was set to Reset_EventHandler(). When I put breakpoint in main() function and try to run the system loops at the constant section of the binary.Basically I am able to download the binary but not able to debug the binary.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 05:58:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-debug-using-Lauterbach-JTAG/m-p/873031#M132622</guid>
      <dc:creator>vmuthusu</dc:creator>
      <dc:date>2019-01-16T05:58:42Z</dc:date>
    </item>
  </channel>
</rss>