<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8M heat problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872828#M132595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using the i.MX8M (Quad) in a product connected to a 1080p LVDS display. We use Yocto as build system and a QT WebEngine based browser running in kiosk mode under Weston.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we bring up a webpage in the browser and start scrolling the page (doesn't matter how simple the page is) after a short time (less than a minute) the GPU is overheated and the kernel reports:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;[  930.557040] hantro receive hot notification event: 1
[  930.562170] System is too hot. GPU3D will work at 1/64 clock&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a passive heat-sink attached to the CPU and no real CPU/GPU load except for the browser. With no user interaction the CPU temperature is ~70 C degrees and under interactions it goes up to around ~84 C before the GPU clock is decreased to 1/64.&lt;/P&gt;&lt;P&gt;Even if the browser is not running the CPU is idling on ~70 C degrees.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have experienced the same problem with both a 4.9 kernel (Yocto Morty based build) and a newer 4.14 (Yocto Sumo based).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else successfully used i.MX8M in a similar setup using passive cooling?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be done to lower the heat/power consumption?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Olle&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jan 2019 10:31:47 GMT</pubDate>
    <dc:creator>ollesandberg</dc:creator>
    <dc:date>2019-01-30T10:31:47Z</dc:date>
    <item>
      <title>i.MX8M heat problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872828#M132595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using the i.MX8M (Quad) in a product connected to a 1080p LVDS display. We use Yocto as build system and a QT WebEngine based browser running in kiosk mode under Weston.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we bring up a webpage in the browser and start scrolling the page (doesn't matter how simple the page is) after a short time (less than a minute) the GPU is overheated and the kernel reports:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;[  930.557040] hantro receive hot notification event: 1
[  930.562170] System is too hot. GPU3D will work at 1/64 clock&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a passive heat-sink attached to the CPU and no real CPU/GPU load except for the browser. With no user interaction the CPU temperature is ~70 C degrees and under interactions it goes up to around ~84 C before the GPU clock is decreased to 1/64.&lt;/P&gt;&lt;P&gt;Even if the browser is not running the CPU is idling on ~70 C degrees.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have experienced the same problem with both a 4.9 kernel (Yocto Morty based build) and a newer 4.14 (Yocto Sumo based).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else successfully used i.MX8M in a similar setup using passive cooling?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be done to lower the heat/power consumption?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Olle&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 10:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872828#M132595</guid>
      <dc:creator>ollesandberg</dc:creator>
      <dc:date>2019-01-30T10:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M heat problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872829#M132596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to test on NXP reference board, i.MX8M EVK with Demo Images on below link&lt;/P&gt;&lt;P&gt;and compare results with custom board. With a small form factor and low copper content,&lt;/P&gt;&lt;P&gt;compared with reference board, on custom board board heat dissipation can be issue.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_MX8MQ&amp;amp;appType=license&amp;amp;location=null" target="_blank"&gt;Linux Binary Demo Files - i.MX 8MQuad EVK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Schematics &lt;BR /&gt;Design Files for the i.MX 8M Evaluation Kit (EVK)&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK?tab=Design_Tools_Tab" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK?tab=Design_Tools_Tab"&gt;i.MX 8M Evaluation Kit|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some figures can be found in AN12118 i.MX8M Quad Power Consumption Measurement, &lt;/P&gt;&lt;P&gt;Coremark test, about 2W dissipation, die temperature = 60C, ambient temperature = 25 C.&lt;/P&gt;&lt;P&gt;KANZI test, about 3W dissipation die temperature = 67C, ambient temperature = 26 C.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/nxp/application-notes/AN12118.pdf" title="https://www.nxp.com/docs/en/nxp/application-notes/AN12118.pdf"&gt;https://www.nxp.com/docs/en/nxp/application-notes/AN12118.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note, current greatly depends on temperature as described in&lt;/P&gt;&lt;P&gt;AN5381 Measuring Current in i.MX Applications sect.6.2. Current vs. ambient temperature&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5381.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN5381.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;AN4579 Thermal Management Guidelines shows various thermal solutions &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4579.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4579.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 05:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872829#M132596</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-31T05:17:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M heat problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872830#M132597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Do You use the recent i.MX8M silicon rev?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 08:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872830#M132597</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-01-31T08:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M heat problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872831#M132598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Don't think we've got the most recent one yet. Is it supposed to lower the power consumption?&lt;/P&gt;&lt;P&gt;Is that the silicon used for the benchmarks in the post above?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 08:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872831#M132598</guid>
      <dc:creator>ollesandberg</dc:creator>
      <dc:date>2019-01-31T08:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M heat problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872832#M132599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olle,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did you solve the problem?&lt;/P&gt;&lt;P&gt;We have nearly the same issue. We have a sumo configuration with no additional software or drivers, but the board is shutting down after a 25min cause of overheating. We tried several setups without heatsink but everytime the board is shutting down. Morty gives us better results than sumo, but not enough space for our applications. We can not accept the board shutting down in idle. So we need an solution for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Tobias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 12:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-heat-problem/m-p/872832#M132599</guid>
      <dc:creator>tobias_wahl</dc:creator>
      <dc:date>2020-03-03T12:58:10Z</dc:date>
    </item>
  </channel>
</rss>