<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IPU V3 Linux-Driver supporting RGB24 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IPU-V3-Linux-Driver-supporting-RGB24/m-p/872269#M132551</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a discovery (for me) which I don't really understand:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom i.MX6 Board with a i.MX6Solo connected to a 24-Bit RGB display.&lt;/P&gt;&lt;P&gt;I'm running a 4.19.26 Mainline Linux-Kernel on it and configured it with the device tree attched to this message (graphic.dtsi).&lt;/P&gt;&lt;P&gt;The I displayed some color gradients on it (attached All-Colors-800x480.png).&lt;/P&gt;&lt;P&gt;But the color gradients don't look as smooth as a 24Bit-color display should look like, they are very visible graded.&lt;/P&gt;&lt;P&gt;So I meassured the output signals and wondered what I saw:&lt;BR /&gt;The lowest bits R0, R1 and R2 are copies of the highest bits R5, R6 and R7. On blue it's the same.&lt;/P&gt;&lt;P&gt;On green only G0 and G1 are copies of higher bits.&lt;/P&gt;&lt;P&gt;So my colors seem to be reduced to &lt;STRONG&gt;RGB565.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something wrong with the IPU-Driver? Am I configuring it the wrong way? How can I enable real 24bit colors?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Mar 2019 07:32:06 GMT</pubDate>
    <dc:creator>steffendoster</dc:creator>
    <dc:date>2019-03-20T07:32:06Z</dc:date>
    <item>
      <title>IPU V3 Linux-Driver supporting RGB24</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-V3-Linux-Driver-supporting-RGB24/m-p/872269#M132551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a discovery (for me) which I don't really understand:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom i.MX6 Board with a i.MX6Solo connected to a 24-Bit RGB display.&lt;/P&gt;&lt;P&gt;I'm running a 4.19.26 Mainline Linux-Kernel on it and configured it with the device tree attched to this message (graphic.dtsi).&lt;/P&gt;&lt;P&gt;The I displayed some color gradients on it (attached All-Colors-800x480.png).&lt;/P&gt;&lt;P&gt;But the color gradients don't look as smooth as a 24Bit-color display should look like, they are very visible graded.&lt;/P&gt;&lt;P&gt;So I meassured the output signals and wondered what I saw:&lt;BR /&gt;The lowest bits R0, R1 and R2 are copies of the highest bits R5, R6 and R7. On blue it's the same.&lt;/P&gt;&lt;P&gt;On green only G0 and G1 are copies of higher bits.&lt;/P&gt;&lt;P&gt;So my colors seem to be reduced to &lt;STRONG&gt;RGB565.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something wrong with the IPU-Driver? Am I configuring it the wrong way? How can I enable real 24bit colors?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 07:32:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-V3-Linux-Driver-supporting-RGB24/m-p/872269#M132551</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2019-03-20T07:32:06Z</dc:date>
    </item>
    <item>
      <title>Re: IPU V3 Linux-Driver supporting RGB24</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-V3-Linux-Driver-supporting-RGB24/m-p/872270#M132552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the chapter&amp;nbsp; 4.11.10.4 IPU Display Interface Signal Mapping of datasheet:&lt;SPAN style="left: 90px; top: 617.091px; font-size: 21.6px; font-family: sans-serif; transform: scaleX(0.985914);"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf" title="https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;pls check if your settings is corrct or not&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 08:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-V3-Linux-Driver-supporting-RGB24/m-p/872270#M132552</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-03-26T08:25:42Z</dc:date>
    </item>
  </channel>
</rss>