<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: USB Ports</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Ports/m-p/872021#M132517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The pinout availability will depend of the used board. In case of requiring more Host ports and you only have one, you may use an external HUB (just considering power requirements).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For additional details regarding USB controllers and configuration, you could take a look to application note AN4589 “&lt;A href="https://www.nxp.com/docs/en/application-note/AN4589.pdf"&gt;Configuring USB on i.MX 6 Series Processors&lt;/A&gt;”.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Mar 2019 00:03:50 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2019-03-20T00:03:50Z</dc:date>
    <item>
      <title>USB Ports</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Ports/m-p/872020#M132516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In iMx6 &amp;nbsp;dual, we noticed we have 4 usb ports( One USB 2.0 OTG and 3 USB2.0 hosts)&lt;/P&gt;&lt;P&gt;but we can able to see the pin out only for one USB 2.0 OTG and One HOST.&lt;/P&gt;&lt;P&gt;I hope if we need two more host do I need to drive through USB HUB or how can I do that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 20:41:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Ports/m-p/872020#M132516</guid>
      <dc:creator>mylsamy_m</dc:creator>
      <dc:date>2019-03-19T20:41:06Z</dc:date>
    </item>
    <item>
      <title>Re: USB Ports</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Ports/m-p/872021#M132517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The pinout availability will depend of the used board. In case of requiring more Host ports and you only have one, you may use an external HUB (just considering power requirements).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For additional details regarding USB controllers and configuration, you could take a look to application note AN4589 “&lt;A href="https://www.nxp.com/docs/en/application-note/AN4589.pdf"&gt;Configuring USB on i.MX 6 Series Processors&lt;/A&gt;”.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 00:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Ports/m-p/872021#M132517</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-03-20T00:03:50Z</dc:date>
    </item>
  </channel>
</rss>