<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: which function loads the kernel image into RAM in imx6q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/which-function-loads-the-kernel-image-into-RAM-in-imx6q/m-p/871863#M132487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Laxman Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BSP uses the bootm command to load the kernel into memory. You can find more about this format and u-boot in general in u-boot’s Reference Manual:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.denx.de/wiki/DULG/Manual"&gt;https://www.denx.de/wiki/DULG/Manual&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Jan 2019 21:26:16 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-01-14T21:26:16Z</dc:date>
    <item>
      <title>which function loads the kernel image into RAM in imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-function-loads-the-kernel-image-into-RAM-in-imx6q/m-p/871862#M132486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;im working on imx6qsabresd&amp;nbsp;&lt;/P&gt;&lt;P&gt;My requirement is stop the uboot at kernel loading into the RAM. because i want to check the battery and power key press.&lt;/P&gt;&lt;P&gt;In which function of uboot can i stop&amp;nbsp; kernel image to load into RAM. i want to stop the function which is loading kernel image into RAM.&lt;/P&gt;&lt;P&gt;Please help me..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;laxman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 10:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-function-loads-the-kernel-image-into-RAM-in-imx6q/m-p/871862#M132486</guid>
      <dc:creator>laxmankumar</dc:creator>
      <dc:date>2019-01-14T10:19:53Z</dc:date>
    </item>
    <item>
      <title>Re: which function loads the kernel image into RAM in imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-function-loads-the-kernel-image-into-RAM-in-imx6q/m-p/871863#M132487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Laxman Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BSP uses the bootm command to load the kernel into memory. You can find more about this format and u-boot in general in u-boot’s Reference Manual:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.denx.de/wiki/DULG/Manual"&gt;https://www.denx.de/wiki/DULG/Manual&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 21:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-function-loads-the-kernel-image-into-RAM-in-imx6q/m-p/871863#M132487</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-01-14T21:26:16Z</dc:date>
    </item>
  </channel>
</rss>