<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How do imx6ul-evk boot from QSPI?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871785#M132482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Jan 2019 01:37:03 GMT</pubDate>
    <dc:creator>zhangbin_eos</dc:creator>
    <dc:date>2019-01-21T01:37:03Z</dc:date>
    <item>
      <title>How do imx6ul-evk boot from QSPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871783#M132480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In imx6ul evk, there is an N25Q256 device. I want to boot from this device.I used L4.1.15_2.0.0-ga_mfg-tools and mfgtool2-yocto-mx-evk-qspi-nor-n25q256a.vbs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;SW602 is set to OFF ON and SW601 is set to OFF OFF &lt;SPAN&gt;OFF OFF&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;2. run&amp;nbsp;&lt;SPAN&gt;mfgtool2-yocto-mx-evk-qspi-nor-n25q256a.vbs. Burn finish and display "Done"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.&amp;nbsp;SW602 is set to&amp;nbsp;ON OFF&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4. Remove SD card&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;5. Power on and debug uart display :&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:36:22 -0500)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 36C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;SF: Detected N25Q256 with page size 256 Bytes, erase size 64 KiB, total 32 MiB&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: FEC1&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0 &lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;MMC: no card present&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;Booting from net ...&lt;BR /&gt;FEC1 Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;BR /&gt;BOOTP broadcast 1&lt;BR /&gt;BOOTP broadcast 2&lt;BR /&gt;BOOTP broadcast 3&lt;BR /&gt;BOOTP broadcast 4&lt;BR /&gt;BOOTP broadcast 5&lt;BR /&gt;BOOTP broadcast 6&lt;BR /&gt;BOOTP broadcast 7&lt;BR /&gt;BOOTP broadcast 8&lt;BR /&gt;BOOTP broadcast 9&lt;BR /&gt;BOOTP broadcast 10&lt;BR /&gt;BOOTP broadcast 11&lt;BR /&gt;BOOTP broadcast 12&lt;BR /&gt;BOOTP broadcast 13&lt;BR /&gt;BOOTP broadcast 14&lt;BR /&gt;BOOTP broadcast 15&lt;BR /&gt;BOOTP broadcast 16&lt;BR /&gt;BOOTP broadcast 17&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dose&amp;nbsp; iMX6UL-evk&amp;nbsp; support this boot mode? If so, how can I set it up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 05:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871783#M132480</guid>
      <dc:creator>zhangbin_eos</dc:creator>
      <dc:date>2019-01-14T05:21:55Z</dc:date>
    </item>
    <item>
      <title>Re: How do imx6ul-evk boot from QSPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871784#M132481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the boot mode is supported but in default settings MFG tool sends only U-Boot to QSPI device. In the ucl.xml file, you can find that the commands used for sending the kernel, device tree&amp;nbsp;and rootfs are missing. This is because QSPI devices usually have too small capacity for the entire image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 16:24:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871784#M132481</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-01-17T16:24:07Z</dc:date>
    </item>
    <item>
      <title>Re: How do imx6ul-evk boot from QSPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871785#M132482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 01:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-imx6ul-evk-boot-from-QSPI/m-p/871785#M132482</guid>
      <dc:creator>zhangbin_eos</dc:creator>
      <dc:date>2019-01-21T01:37:03Z</dc:date>
    </item>
  </channel>
</rss>