<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: apt-get not found in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/apt-get-not-found/m-p/870753#M132382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Varun K,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SBC IMX6 Pico ITX is not supported on the NXP BSP Release so I would recommend looking at this board BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this board BSP is based on Yocto you can add package management to the image and the apt function by adding the following commands to the conf/local.conf file. You would then need to configure the repository list for apt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += "package-management"&lt;/P&gt;&lt;P&gt;CORE_IMAGE_EXTRA_INSTALL += "apt"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 20:37:16 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-01-11T20:37:16Z</dc:date>
    <item>
      <title>apt-get not found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-get-not-found/m-p/870752#M132381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using SBC IMX6 Pico ITX, Linux 3.10 with yocto distribution. But I'm unable to install any package,as the apt-get command is not working in my&amp;nbsp; SBC IMX6.&lt;/P&gt;&lt;P&gt;How do I install apt-get in my SBC IMX6 Pico ITX to get packages?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 11:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-get-not-found/m-p/870752#M132381</guid>
      <dc:creator>kvk0422</dc:creator>
      <dc:date>2019-01-11T11:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: apt-get not found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-get-not-found/m-p/870753#M132382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Varun K,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SBC IMX6 Pico ITX is not supported on the NXP BSP Release so I would recommend looking at this board BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this board BSP is based on Yocto you can add package management to the image and the apt function by adding the following commands to the conf/local.conf file. You would then need to configure the repository list for apt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += "package-management"&lt;/P&gt;&lt;P&gt;CORE_IMAGE_EXTRA_INSTALL += "apt"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 20:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-get-not-found/m-p/870753#M132382</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-01-11T20:37:16Z</dc:date>
    </item>
  </channel>
</rss>