<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック yocto  add pam module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-add-pam-module/m-p/870138#M132324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;How can make the&amp;nbsp; pam module to rootfs?&amp;nbsp; i use imx6&amp;nbsp; yocto enviroment!&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. i&amp;nbsp; add this in the&amp;nbsp;local.conf&lt;/P&gt;&lt;P&gt;&amp;nbsp;IMAGE_INSTALL_append += " pam"&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. then,&amp;nbsp; bitbake fsl-image-qt5.&amp;nbsp; &amp;nbsp;and the error :&lt;/P&gt;&lt;P&gt;ERROR: Nothing RPROVIDES 'pam' (but /work/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb RDEPENDS on or otherwise requires it)&lt;BR /&gt;NOTE: Runtime target 'pam' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['pam']&lt;BR /&gt;ERROR: Required build target 'fsl-image-qt5' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-qt5', 'pam']&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i found&amp;nbsp; pam at path :&amp;nbsp; poky/meta/recipes-extended/pam. but&amp;nbsp; i do not known&amp;nbsp; how to do . is some one&amp;nbsp;&lt;/P&gt;&lt;P&gt;came the same problem.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2019 03:15:44 GMT</pubDate>
    <dc:creator>1074562799</dc:creator>
    <dc:date>2019-02-19T03:15:44Z</dc:date>
    <item>
      <title>yocto  add pam module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-add-pam-module/m-p/870138#M132324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;How can make the&amp;nbsp; pam module to rootfs?&amp;nbsp; i use imx6&amp;nbsp; yocto enviroment!&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1. i&amp;nbsp; add this in the&amp;nbsp;local.conf&lt;/P&gt;&lt;P&gt;&amp;nbsp;IMAGE_INSTALL_append += " pam"&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. then,&amp;nbsp; bitbake fsl-image-qt5.&amp;nbsp; &amp;nbsp;and the error :&lt;/P&gt;&lt;P&gt;ERROR: Nothing RPROVIDES 'pam' (but /work/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb RDEPENDS on or otherwise requires it)&lt;BR /&gt;NOTE: Runtime target 'pam' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['pam']&lt;BR /&gt;ERROR: Required build target 'fsl-image-qt5' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-qt5', 'pam']&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i found&amp;nbsp; pam at path :&amp;nbsp; poky/meta/recipes-extended/pam. but&amp;nbsp; i do not known&amp;nbsp; how to do . is some one&amp;nbsp;&lt;/P&gt;&lt;P&gt;came the same problem.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 03:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-add-pam-module/m-p/870138#M132324</guid>
      <dc:creator>1074562799</dc:creator>
      <dc:date>2019-02-19T03:15:44Z</dc:date>
    </item>
    <item>
      <title>Re:  yocto  add pam module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-add-pam-module/m-p/870139#M132325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 海 陈&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at nxp yocto guidelines:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1616"&gt;Freescale Yocto Project main page&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100203"&gt;BSP porting guide: from a I.mx6q reference Board to a Custom board (in Yocto project)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95333"&gt;Task #10 - How to create a custom layer&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 10:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-add-pam-module/m-p/870139#M132325</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-19T10:38:49Z</dc:date>
    </item>
  </channel>
</rss>