<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Quad SPI boot on iMX7D</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869356#M132214</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The QuadSPI boot configuration can be found in section 6.6.6 of the i.MX7D Reference Manual. You can set it using the GPIO boot configuration or set it up on fuses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2019 20:38:12 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-02-19T20:38:12Z</dc:date>
    <item>
      <title>Quad SPI boot on iMX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869355#M132213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I could understand Quad SPI block supports 2 Quad SPI interfaces with 2 Chip selects for each one of them. Overall 4 serial devices can be used. My question is how specific Quad SPI device is configured as a boot source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Feb 2019 14:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869355#M132213</guid>
      <dc:creator>syuriks</dc:creator>
      <dc:date>2019-02-17T14:31:28Z</dc:date>
    </item>
    <item>
      <title>Re: Quad SPI boot on iMX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869356#M132214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The QuadSPI boot configuration can be found in section 6.6.6 of the i.MX7D Reference Manual. You can set it using the GPIO boot configuration or set it up on fuses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 20:38:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869356#M132214</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-02-19T20:38:12Z</dc:date>
    </item>
    <item>
      <title>Re: Quad SPI boot on iMX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869357#M132215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've read QuadSPI boot configuration section and I understand that it can be set up by using fuses or GPIOs. The only question is how to select specific QuadSPI device from 2 connected devices. In section 10.2.1.2.1 QuadSPI Normal Mode of Operation it is stated that 2 external flashes can be accessed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 09:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-SPI-boot-on-iMX7D/m-p/869357#M132215</guid>
      <dc:creator>syuriks</dc:creator>
      <dc:date>2019-02-21T09:59:00Z</dc:date>
    </item>
  </channel>
</rss>