<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error in i.MX8M Mini pintool/checklist in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-i-MX8M-Mini-pintool-checklist/m-p/868941#M132181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm making a review of a i.MX8M Mini (MIMX8MM6CVTKZ) but there is a error in the pintool.&lt;/P&gt;&lt;P&gt;P1 is DRAM_ZN, P2 is DRAM_ZN_SENSE, P5 is DRAM_VREF in the tool but in the datasheet of the device P1 is&amp;nbsp; DRAM_VREF and P2 is DRAM_ZN&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the design checklist there is also a problem with DDR4, in IMX8MMHDG.pdf REV. 0 02/2019 table 4 the first point it is said that ZQ should be connected to AA13 while AA13 is a VSS pin in the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Apr 2019 12:15:20 GMT</pubDate>
    <dc:creator>koenvercammen</dc:creator>
    <dc:date>2019-04-01T12:15:20Z</dc:date>
    <item>
      <title>Error in i.MX8M Mini pintool/checklist</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-i-MX8M-Mini-pintool-checklist/m-p/868941#M132181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm making a review of a i.MX8M Mini (MIMX8MM6CVTKZ) but there is a error in the pintool.&lt;/P&gt;&lt;P&gt;P1 is DRAM_ZN, P2 is DRAM_ZN_SENSE, P5 is DRAM_VREF in the tool but in the datasheet of the device P1 is&amp;nbsp; DRAM_VREF and P2 is DRAM_ZN&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the design checklist there is also a problem with DDR4, in IMX8MMHDG.pdf REV. 0 02/2019 table 4 the first point it is said that ZQ should be connected to AA13 while AA13 is a VSS pin in the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2019 12:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-i-MX8M-Mini-pintool-checklist/m-p/868941#M132181</guid>
      <dc:creator>koenvercammen</dc:creator>
      <dc:date>2019-04-01T12:15:20Z</dc:date>
    </item>
    <item>
      <title>Re: Error in i.MX8M Mini pintool/checklist</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-i-MX8M-Mini-pintool-checklist/m-p/868942#M132182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Koen,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for pointing out these errors. The Pintool has been fixed and the hardware design guide should be also fixed on the next release of the documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 17:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-i-MX8M-Mini-pintool-checklist/m-p/868942#M132182</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-06-28T17:24:26Z</dc:date>
    </item>
  </channel>
</rss>