<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8qxp pcie init fail. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868594#M132146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好，我根据你说的修改后PLL是锁了，但还是会初始化失败&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82543i829A9D0318C7526E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;能否贴一下你的dts部分呢&lt;/P&gt;&lt;P&gt;谢谢~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Jul 2019 09:32:23 GMT</pubDate>
    <dc:creator>liuhongbo1</dc:creator>
    <dc:date>2019-07-31T09:32:23Z</dc:date>
    <item>
      <title>imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868589#M132141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;imx8qxp , I want to use PCIE,but&amp;nbsp; init fail,Please help to slove it.thank you.&lt;/P&gt;&lt;P&gt;[ 2.088471] OF: PCI: host bridge /pcie@0x5f010000 ranges:&lt;BR /&gt;[ 2.093633] OF: PCI: No bus range found for /pcie@0x5f010000, using [bus 00-ff]&lt;BR /&gt;[ 2.101031] OF: PCI: IO 0x7ff80000..0x7ff8ffff -&amp;gt; 0x00000000&lt;BR /&gt;[ 2.106928] OF: PCI: MEM 0x70000000..0x7fefffff -&amp;gt; 0x70000000&lt;BR /&gt;[ 2.115132] imx-pcie 5f010000.pcie: ERROR PM_REQ_CORE_RST is still set.&lt;BR /&gt;[ 2.122458] imx-pcie 5f010000.pcie: pcie phy pll can't be locked.&lt;BR /&gt;[ 2.168236] imx-pcie 5f010000.pcie: failed to initialize host&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 12:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868589#M132141</guid>
      <dc:creator>健谭谭</dc:creator>
      <dc:date>2019-01-10T12:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868590#M132142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 健 谭&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately so far there is no hardware guide document for that part (it is still preproduction),&lt;/P&gt;&lt;P&gt;Some preliminary pcie check points: check AC coupling at each transmitter (use a 0.22 μF cap on both the &lt;BR /&gt;PCIE_TXP and PCIE_TXN outputs). The receiver must be DC coupled.&lt;BR /&gt;Check voltages on VDD_PCIE0_1P0, VDD_PCIE1_1P0, &lt;BR /&gt;PCIE_REF_QR ball should be connected to ground through a 453 Ω, 1% resistor,&lt;BR /&gt;PCIE_REXT ball should be connected to the PCIE0_PHY_PLL_REF_RETURN &lt;BR /&gt;ball through an 845 Ω, 0.5% resistor.&lt;/P&gt;&lt;P&gt;One can try with i.MX8QXP Demo files&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_MX8QXP&amp;amp;appType=license&amp;amp;location=null" title="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_MX8QXP&amp;amp;appType=license&amp;amp;location=null"&gt;https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_MX8QXP&amp;amp;appType=license&amp;amp;location=null&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;use Linux L4.14.78_1.0.0 &lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga" rel="nofollow" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 23:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868590#M132142</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-10T23:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868591#M132143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 06:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868591#M132143</guid>
      <dc:creator>健谭谭</dc:creator>
      <dc:date>2019-01-14T06:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868592#M132144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;您好，我也遇到了同样的问题，请问一下是怎么解决的，谢谢！&lt;/P&gt;&lt;P&gt;我的原理图：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85871iF8BDE35ACE11F71B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;我的启动logo如下：&lt;/P&gt;&lt;P&gt;[ 0.948995] OF: PCI: host bridge /pcie@0x5f010000 ranges:&lt;BR /&gt;[ 0.949005] OF: PCI: No bus range found for /pcie@0x5f010000, using [bus 00-ff]&lt;BR /&gt;[ 0.949018] OF: PCI: IO 0x7ff80000..0x7ff8ffff -&amp;gt; 0x00000000&lt;BR /&gt;[ 0.949033] OF: PCI: MEM 0x70000000..0x7fefffff -&amp;gt; 0x70000000&lt;BR /&gt;[ 0.951582] imx6q-pcie 5f010000.pcie: ERROR PM_REQ_CORE_RST is still set.&lt;BR /&gt;[ 0.972396] imx6q-pcie 5f010000.pcie: pcie phy pll can't be locked.&lt;BR /&gt;[ 1.012421] imx6q-pcie 5f010000.pcie: failed to initialize host&lt;BR /&gt;[ 1.012426] imx6q-pcie 5f010000.pcie: unable to add pcie port.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 03:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868592#M132144</guid>
      <dc:creator>baiseyuzhou</dc:creator>
      <dc:date>2019-06-11T03:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868593#M132145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;imx-scfw-porting-kit-0.7/mx8qx_b0/scfw_export_mx8qx/platform/board/mx8qx_mek/board.c&lt;/P&gt;&lt;P&gt;         /* Used whenever HSIO SS powered up. Valid return values are&lt;/P&gt;&lt;P&gt;            BOARD_PARM_RTN_EXTERNAL or BOARD_PARM_RTN_INTERNAL */&lt;/P&gt;&lt;P&gt;         case BOARD_PARM_PCIE_PLL :&lt;/P&gt;&lt;P&gt;-            rtn = BOARD_PARM_RTN_EXTERNAL;&lt;/P&gt;&lt;P&gt;+            rtn = BOARD_PARM_RTN_INTERNAL;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;重新生成scfw_tcm.bin。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 07:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868593#M132145</guid>
      <dc:creator>健谭谭</dc:creator>
      <dc:date>2019-06-19T07:29:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868594#M132146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好，我根据你说的修改后PLL是锁了，但还是会初始化失败&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82543i829A9D0318C7526E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;能否贴一下你的dts部分呢&lt;/P&gt;&lt;P&gt;谢谢~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 09:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868594#M132146</guid>
      <dc:creator>liuhongbo1</dc:creator>
      <dc:date>2019-07-31T09:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868595#M132147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Can you show your schematic for more detail about pcie ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Then you can refer to it.&amp;nbsp;&lt;A href="https://community.nxp.com/message/1115151"&gt;https://community.nxp.com/message/1115151&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2019 02:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868595#M132147</guid>
      <dc:creator>gnar_fang</dc:creator>
      <dc:date>2019-09-23T02:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868596#M132148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;您好！&lt;/P&gt;&lt;P&gt;我也遇到了和您一样的问题，log一模一样，请问您最后是怎么解决的呢？&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;能否贴一下你的dts部分呢？&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;谢谢!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 09:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868596#M132148</guid>
      <dc:creator>liuzhi</dc:creator>
      <dc:date>2020-05-18T09:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868597#M132149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你还，是硬件电路的问题，pcie两根线要加下拉电阻，具体你可以咨询代理商。提供解决方案。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 01:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868597#M132149</guid>
      <dc:creator>健谭谭</dc:creator>
      <dc:date>2020-05-20T01:50:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868598#M132150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;感谢回复！&lt;/P&gt;&lt;P&gt;我们使用的是外部clk,外部clk的话pcie两根线不用加下拉电阻对吗？&lt;/P&gt;&lt;P&gt;请问还有什么原因为出现这样的log呢？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 08:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868598#M132150</guid>
      <dc:creator>liuzhi</dc:creator>
      <dc:date>2020-05-20T08:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868599#M132151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;使用外部clk，不用。 你有demo板吗，用demo板，对比测量一下信号。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 02:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868599#M132151</guid>
      <dc:creator>健谭谭</dc:creator>
      <dc:date>2020-05-22T02:10:49Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp pcie init fail.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868600#M132152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;感谢帮助，问题已经解决，对比发现是外部给imx8的clk不稳定导致的。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 06:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-pcie-init-fail/m-p/868600#M132152</guid>
      <dc:creator>liuzhi</dc:creator>
      <dc:date>2020-05-28T06:34:43Z</dc:date>
    </item>
  </channel>
</rss>