<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX6ul JTAG eFUSE programming</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867431#M131989</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;thanks for the answer. Then please let me ask a broader question.&lt;/P&gt;&lt;P&gt;Is there a JTAG flash tool for the i.MX6 UL in general? Something we can use in our production process if USB is not available?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 07:04:58 GMT</pubDate>
    <dc:creator>patrick_schneid</dc:creator>
    <dc:date>2019-01-11T07:04:58Z</dc:date>
    <item>
      <title>i.MX6ul JTAG eFUSE programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867429#M131987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I have a (hopefully) simple question. We have a custom board with i.MX6ul controller, a JTAG connection and a ARM ULINK pro device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to program the eFUSEs via JTAG with the ULINK pro device and if so, what software is used for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that it is recommended to use the NXP U-Boot software to program the fuses and that case is well tested and functional with our hardware&amp;nbsp;- but we have use cases where we need to use the raw JTAG without UBoot already running on the device and without the USB-Bootloader and MFGTools.&lt;/P&gt;&lt;P&gt;Is that possible and what software is used?&lt;/P&gt;&lt;P&gt;Thank you guys and regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 11:16:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867429#M131987</guid>
      <dc:creator>patrick_schneid</dc:creator>
      <dc:date>2019-01-10T11:16:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ul JTAG eFUSE programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867430#M131988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of jtag scripts or tools for fuse programming, but&lt;/P&gt;&lt;P&gt;for adding fuse programming script commands one can look at baremetal sdk ocotp example&lt;/P&gt;&lt;P&gt;(OCOTP controller is similar to i.MX6Q),&amp;nbsp; 1.1.0_iMX6_Platform_SDK.zip available on &lt;A href="https://community.nxp.com/thread/432859"&gt;SMP Enable in IMX6&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 00:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867430#M131988</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-11T00:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ul JTAG eFUSE programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867431#M131989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;thanks for the answer. Then please let me ask a broader question.&lt;/P&gt;&lt;P&gt;Is there a JTAG flash tool for the i.MX6 UL in general? Something we can use in our production process if USB is not available?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 07:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867431#M131989</guid>
      <dc:creator>patrick_schneid</dc:creator>
      <dc:date>2019-01-11T07:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ul JTAG eFUSE programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867432#M131990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sorry there is no JTAG flash tool for the i.MX6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jan 2019 00:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867432#M131990</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-12T00:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ul JTAG eFUSE programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867433#M131991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need same possibility - set boot mode via J-link for custom SoM without Usb connector at our mass production line. I need write BOOT_CFG1/2/4 efuses using JTAG interface. Does it possible at all?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Apr 2020 13:36:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ul-JTAG-eFUSE-programming/m-p/867433#M131991</guid>
      <dc:creator>almaz1c</dc:creator>
      <dc:date>2020-04-04T13:36:53Z</dc:date>
    </item>
  </channel>
</rss>