<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSAIF2 interrupt on iMX233 (WINCE6 R3)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SAIF2-interrupt-on-iMX233-WINCE6-R3/m-p/213488#M13189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to get SAIF2 up and running on a iMX233. I see that the DMA command complete interrupt is set after a DMA transfer, but my thread is not serviced. If I do the same with SAIF1 everything works fine. (SAIF1is using another interrupt number)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anyone ho has ever tried using SAIF2 on an iMX233 or any suggestions to debug the interrupt piece from dma to interrupt controller?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maarten.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2012 10:49:04 GMT</pubDate>
    <dc:creator>MenM</dc:creator>
    <dc:date>2012-02-22T10:49:04Z</dc:date>
    <item>
      <title>SAIF2 interrupt on iMX233 (WINCE6 R3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SAIF2-interrupt-on-iMX233-WINCE6-R3/m-p/213488#M13189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to get SAIF2 up and running on a iMX233. I see that the DMA command complete interrupt is set after a DMA transfer, but my thread is not serviced. If I do the same with SAIF1 everything works fine. (SAIF1is using another interrupt number)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anyone ho has ever tried using SAIF2 on an iMX233 or any suggestions to debug the interrupt piece from dma to interrupt controller?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maarten.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2012 10:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SAIF2-interrupt-on-iMX233-WINCE6-R3/m-p/213488#M13189</guid>
      <dc:creator>MenM</dc:creator>
      <dc:date>2012-02-22T10:49:04Z</dc:date>
    </item>
  </channel>
</rss>