<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Boot from Serial flash in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-Serial-flash/m-p/865922#M131885</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 麻生 淳一&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;dose the serial flash with hardware reset pin have to be introduced, and resetting&lt;/P&gt;&lt;P&gt;&amp;gt;the serial flash when i.MX6 is rebooting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this is correct idea.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jan 2019 23:04:47 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-01-28T23:04:47Z</dc:date>
    <item>
      <title>Boot from Serial flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-Serial-flash/m-p/865921#M131884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i.MX6 is accidentally&amp;nbsp;restarted during accessing to&amp;nbsp;the serial flash&amp;nbsp;at upper 128Mb segment with 4-byte addressing mode.&lt;/P&gt;&lt;P&gt;Then i.MX6 tries to reboot from the serial flash with 3-byte addressing mode but the serial flash&amp;nbsp;still stays in 4-byte addressing mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this case,&amp;nbsp;the serial flash can not be read correctly because there are mismatch of addressing mode&amp;nbsp;between i.MX6 and serial flash.&lt;/P&gt;&lt;P&gt;To avoid this kind of issue, dose the serial flash with hardware reset pin have to be introduced, and resetting the serial flash when i.MX6 is rebooting?&lt;/P&gt;&lt;P&gt;Or are there any other&amp;nbsp;idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;JA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 03:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-Serial-flash/m-p/865921#M131884</guid>
      <dc:creator>asou_junichi</dc:creator>
      <dc:date>2019-01-28T03:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from Serial flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-Serial-flash/m-p/865922#M131885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 麻生 淳一&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;dose the serial flash with hardware reset pin have to be introduced, and resetting&lt;/P&gt;&lt;P&gt;&amp;gt;the serial flash when i.MX6 is rebooting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this is correct idea.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 23:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-Serial-flash/m-p/865922#M131885</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-28T23:04:47Z</dc:date>
    </item>
  </channel>
</rss>