<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Speed of Flash Interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865544#M131821</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are right, the SD/eMMC interface of the i.MX8M processor is faster than the Raw NAND interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For SD/eMMC devices, all ECC and other required processing is perfomed within the device, so, there are no special features required from the processor.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Mar 2019 09:29:15 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2019-03-19T09:29:15Z</dc:date>
    <item>
      <title>Speed of Flash Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865543#M131820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have a been looking a solution to provide highest possible NAND Flash interface. imax8m itself having limitation to support TLC etc.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the application processors manual,&lt;/P&gt;&lt;P&gt;eMMC&amp;nbsp; =&amp;gt; DDR mode can support up to 400 Mbytes/sec whereas raw NAND can support up to 200 Mbytes/sec.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Looks like eMMC is faster than raw NAND.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not clear on the ECC etc. Which interface(eMMC or raw NAND) will be having better throughput?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2019 12:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865543#M131820</guid>
      <dc:creator>vinoth_ta</dc:creator>
      <dc:date>2019-03-18T12:32:35Z</dc:date>
    </item>
    <item>
      <title>Re: Speed of Flash Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865544#M131821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are right, the SD/eMMC interface of the i.MX8M processor is faster than the Raw NAND interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For SD/eMMC devices, all ECC and other required processing is perfomed within the device, so, there are no special features required from the processor.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 09:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865544#M131821</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-03-19T09:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: Speed of Flash Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865545#M131822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any application note explain about these information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am interested to know the throughput of raw NAND or eMMC. I would need &lt;/P&gt;&lt;P&gt;to select the device which is having better throughput.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vinoth TA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 12:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865545#M131822</guid>
      <dc:creator>vinoth_ta</dc:creator>
      <dc:date>2019-03-19T12:52:33Z</dc:date>
    </item>
    <item>
      <title>Re: Speed of Flash Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865546#M131823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no separate Application Note document for that. Please refer to the numbers, given in the Data Sheet document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 07:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Speed-of-Flash-Interface/m-p/865546#M131823</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-03-20T07:15:41Z</dc:date>
    </item>
  </channel>
</rss>