<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBitbake speed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-speed/m-p/862477#M131564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #242729; background-color: #ffffff;"&gt;I'm working on a project which has many Bitbake recipes and takes a lot of time.(up to 24 hours)&amp;nbsp; I am a newbie on embedded Linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #242729; background-color: #ffffff;"&gt;How can ı solve this problem?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #242729; background-color: #ffffff;"&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Jan 2019 13:53:51 GMT</pubDate>
    <dc:creator>dugurlu</dc:creator>
    <dc:date>2019-01-25T13:53:51Z</dc:date>
    <item>
      <title>Bitbake speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-speed/m-p/862477#M131564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #242729; background-color: #ffffff;"&gt;I'm working on a project which has many Bitbake recipes and takes a lot of time.(up to 24 hours)&amp;nbsp; I am a newbie on embedded Linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #242729; background-color: #ffffff;"&gt;How can ı solve this problem?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #242729; background-color: #ffffff;"&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 13:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-speed/m-p/862477#M131564</guid>
      <dc:creator>dugurlu</dc:creator>
      <dc:date>2019-01-25T13:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-speed/m-p/862478#M131565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dogan Ugurlu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bitbake can take a while especially with recipes with a large number of tasks. It also fetches the source code on-demand, so there are several variables that will affect how much bitbake takes to finish all tasks in the queue:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Your internet connection is one variable, as some repositories are very large.&lt;/P&gt;&lt;P&gt;- If you are using a Virtual Machine the process will be much slower.&lt;/P&gt;&lt;P&gt;- Having multiple cores allow to run several tasks in parallel. You may change this number, but it’s recommended to keep it at 2X the number of cores at a maximum. To do this add these lines on the conf/local.conf file under the build directory (instead of n, place the number of parallel threads you desire):&lt;/P&gt;&lt;P&gt;PARALLEL_MAKE ?= "-j n"&lt;/P&gt;&lt;P&gt;BB_NUMBER_THREADS ?= "n"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 22:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-speed/m-p/862478#M131565</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-01-25T22:03:58Z</dc:date>
    </item>
  </channel>
</rss>