<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861603#M131445</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Petros,&lt;/P&gt;&lt;P&gt;I have already checked the Lattice Solution, and it is surely possible to do it. But the thought remains that would I be needing any additional drivers to drive this Camera Sensor + Converter Chip.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Apr 2019 07:54:18 GMT</pubDate>
    <dc:creator>rvalvekar</dc:creator>
    <dc:date>2019-04-23T07:54:18Z</dc:date>
    <item>
      <title>Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861598#M131440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am researching into interfacing IMX226CQJ with i.MX Processors.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Will I be needing any converter to convert the LVDS Signals from Image Sensor when connecting to the processor ?&lt;/P&gt;&lt;P&gt;2. Are there any leads i can follow, for Linux Drivers for Sony Image Sensors ?&lt;/P&gt;&lt;P&gt;3. Is it necessary to convert LVDS Image Sensor output to MIPI CSI or Parallel Interface ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the sensor is newly designed, there is not much information about it. Would like to get a community support for the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Rohan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 08:09:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861598#M131440</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-01-25T08:09:55Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861599#M131441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rohan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the this new camera has an LVDS interface as input, for sure if you want to connect with the i.MX Processor you would need an extra component,&amp;nbsp; like the&amp;nbsp; LVDS to MIPI&amp;nbsp; converter or&amp;nbsp; LVDS to CSI Parallel interface,&amp;nbsp; by the way,&amp;nbsp; I have never seen such components since the LVDS always has been as outputs, but since you are mention this is new, maybe there is already the converter also.&lt;/P&gt;&lt;P&gt;But I think it is better to use the MIPI Cameras, since it is basically and LVDS regarding the signal conditioning. But I do not know what new advantages would bring this new kind of cameras.&lt;/P&gt;&lt;P&gt;Regarding the software, this would be direct from SONY, since all the cameras has a part of embedded config that cannot change, and it is bring from the manufacturer, so you need to contact SONY to get details about the drivers that they should have.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jaime&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 21:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861599#M131441</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2019-01-25T21:20:31Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861600#M131442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jamie,&lt;/P&gt;&lt;P&gt;Thank you for the reply. After getting some more information about the whole situation. I have some more questions regarding the same topic.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. After having the sub-LVDS signals from the camera sensors converted into Parallel Interface ready signal, I would like to connect it to the Parallel Capture Interface of the i.MX Processor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Linux, I will be needing some drivers for the parallel capture. Do i need to write custom drivers after the data IO has been converted into Parallel Channel ? So do i need to connect with Sensor Bridge Manufacturers for the driver or do i need to custom design the drivers myself ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the only drivers that are available with Linux Kernel are generic or OV based, it is hard to determine the timeline and the exactly driver design method for this sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help,&lt;/P&gt;&lt;P&gt;Rohan&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 15:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861600#M131442</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-01-28T15:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861601#M131443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Hello Jamie,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Thank you for the reply. After getting some more information about the whole situation. I have some more questions regarding the same topic.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;1. After having the sub-LVDS signals from the camera sensors converted into Parallel Interface ready signal, I would like to connect it to the Parallel Capture Interface of the i.MX Processor.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;For Linux, I will be needing some drivers for the parallel capture. Do i need to write custom drivers after the data IO has been converted into Parallel Channel ? So do i need to connect with Sensor Bridge Manufacturers for the driver or do i need to custom design the drivers myself ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Since the only drivers that are available with Linux Kernel are generic or OV based, it is hard to determine the timeline and the exactly driver design method for this sensor.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Thanks for the help,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Rohan&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 12:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861601#M131443</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-01-30T12:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861602#M131444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rohan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if you found a solution on your first question regarding the converter. I am researching this myself as well and found out possbily two solutions. The first solution is to use the Lattice MachXO3 or Crosslink to convert the output. It seems like a great idea until you dive into it. Either you will have to program the conversion yourself or you'll have to buy an IP block (which may cost a lot of money). The second solution which I'm not entirely sure about is using the&amp;nbsp;&lt;A href="https://www.analog.com/media/en/technical-documentation/data-sheets/ADV7782.pdf"&gt;ADV7782&lt;/A&gt;&amp;nbsp;chip to convert the output to CSI-2 (Has been mentioned&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/message/869000?sr=search&amp;amp;searchId=7958ebbc-f138-4310-83ea-bd03322a4a7d&amp;amp;searchIndex=1"&gt;here&lt;/A&gt;). The limited datasheet from the ADV7782 only shows that it&amp;nbsp;has a 5 lane&amp;nbsp;OpenLDI LVDS input. This chip might be a bottleneck for your chip as it most likely will handle up to 1080p60.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 11:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861602#M131444</guid>
      <dc:creator>pks</dc:creator>
      <dc:date>2019-04-11T11:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing IMX226CQJ Image Sensor with i.MX Processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861603#M131445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Petros,&lt;/P&gt;&lt;P&gt;I have already checked the Lattice Solution, and it is surely possible to do it. But the thought remains that would I be needing any additional drivers to drive this Camera Sensor + Converter Chip.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 07:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-IMX226CQJ-Image-Sensor-with-i-MX-Processors/m-p/861603#M131445</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-04-23T07:54:18Z</dc:date>
    </item>
  </channel>
</rss>