<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 eMMC having TLC NAND Flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861372#M131416</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is noted that IMX8M will support MLC,SLC and Toggle NAND flash. Also support eMMC&amp;nbsp; version upto 5.1 (if use latest bsp). I could see high density eMMC5.1&amp;nbsp;may have TLC NAND Flash in it .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shall we still use the eMMC having TLC type of NAND Flash in it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got below response from NXP support&amp;nbsp; "&amp;nbsp;as I known, imx8M can support emmc 5.1" :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vinoth TA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Mar 2019 09:55:27 GMT</pubDate>
    <dc:creator>vinoth_ta</dc:creator>
    <dc:date>2019-03-01T09:55:27Z</dc:date>
    <item>
      <title>eMMC having TLC NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861372#M131416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is noted that IMX8M will support MLC,SLC and Toggle NAND flash. Also support eMMC&amp;nbsp; version upto 5.1 (if use latest bsp). I could see high density eMMC5.1&amp;nbsp;may have TLC NAND Flash in it .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shall we still use the eMMC having TLC type of NAND Flash in it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got below response from NXP support&amp;nbsp; "&amp;nbsp;as I known, imx8M can support emmc 5.1" :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vinoth TA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2019 09:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861372#M131416</guid>
      <dc:creator>vinoth_ta</dc:creator>
      <dc:date>2019-03-01T09:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC having TLC NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861373#M131417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; IMX8M documentation (Reference Manual, DataSheets) state, that eMMC 5.0 is supported.&lt;/P&gt;&lt;P&gt;This means, that devices of eMMC 5.1 can be used as much as they are backward compatible&lt;/P&gt;&lt;P&gt;with eMMC 5.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 08:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861373#M131417</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-03-04T08:00:18Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC having TLC NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861374#M131418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks. Shall we still use the eMMC having TLC type of NAND Flash in it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vinoth TA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 08:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861374#M131418</guid>
      <dc:creator>vinoth_ta</dc:creator>
      <dc:date>2019-03-04T08:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC having TLC NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861375#M131419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;As I understand - specifics of NAND, used in eMMC devices, is internal eMMC issue,&amp;nbsp;&lt;/P&gt;&lt;P&gt;and this does not affect eMMC (external) interface. So, customers can use i.MX8M with&lt;/P&gt;&lt;P&gt;any eMMC, satisfying the 5.0 specs.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2019 04:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-having-TLC-NAND-Flash/m-p/861375#M131419</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-03-05T04:32:59Z</dc:date>
    </item>
  </channel>
</rss>