<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859112#M131206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, NXP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom board with imx6q and sgtl5000, but when the machine get into suspend or wake up or shutdown, the speaker had a "pop" noise. I had tried this: setting the DAC_MUTE_LEFT and DAC_MUTE_RIGHT bit in suspend function, and clear them in resume function, but it didn't works. Any advices? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;bo xu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jan 2019 07:36:12 GMT</pubDate>
    <dc:creator>bakbad</dc:creator>
    <dc:date>2019-01-08T07:36:12Z</dc:date>
    <item>
      <title>iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859112#M131206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, NXP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom board with imx6q and sgtl5000, but when the machine get into suspend or wake up or shutdown, the speaker had a "pop" noise. I had tried this: setting the DAC_MUTE_LEFT and DAC_MUTE_RIGHT bit in suspend function, and clear them in resume function, but it didn't works. Any advices? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;bo xu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 07:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859112#M131206</guid>
      <dc:creator>bakbad</dc:creator>
      <dc:date>2019-01-08T07:36:12Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859113#M131207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi bo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;additionally one can consider decreasing volume as described in&lt;/P&gt;&lt;P&gt;sect.2.2.6 Volume Control AN3663 SGTL5000 Initialization and Programming&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf" title="http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf"&gt;http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 10:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859113#M131207</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-08T10:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859114#M131208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for&amp;nbsp; your advice.I tried as section 2.2.6 told.but when i put the code in sgtl5000_suspend() like this:&lt;/P&gt;&lt;P&gt;static int sgtl5000_suspend(struct snd_soc_codec *codec)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;// Configure ADC left and right analog volume to desired default.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;snd_soc_write(codec, SGTL5000_CHIP_ANA_ADC_CTRL, 0x0000);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;// LINEOUT and DAC volume control&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;snd_soc_update_bits(codec, SGTL5000_CHIP_ANA_CTRL, 8, 0);&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;snd_soc_write(codec, SGTL5000_CHIP_DAC_VOL, 0x3c3c);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;snd_soc_&lt;SPAN&gt;update_bits&lt;/SPAN&gt;&lt;SPAN&gt;(codec, SGTL5000_CHIP_ADCDAC_CTRL, 2, 0);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;snd_soc_&lt;SPAN&gt;update_bits&lt;/SPAN&gt;&lt;SPAN&gt;(codec, SGTL5000_CHIP_ADCDAC_CTRL, 3, 0);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;// Unmute ADC&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;snd_soc_&lt;SPAN&gt;update_bits&lt;/SPAN&gt;&lt;SPAN&gt;(code, SGTL5000_CHIP_ANA_CTRL, 0, 0);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;sgtl5000_set_bias_level(codec, SND_SOC_BIAS_OFF);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;and rebuild the kernel for the machine. But the machine had no sound before i set it to suspend and when the machine got into suspend status, it can't wake up.Did i missed something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;bo xu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 14:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859114#M131208</guid>
      <dc:creator>bakbad</dc:creator>
      <dc:date>2019-01-09T14:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859115#M131209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; solved this problem by closing the amplifier（TS4962）'s STBY pin before the system get into suspend, for letting the machine get into suspend we use commands like this "echo 'mem' &amp;gt; /sys/power/state" in the application layer.&lt;/P&gt;&lt;P&gt;The processes just like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo 0 &amp;gt; /sys/class/gpio/gpio204/value (num 204 is the pin number of TS4962's STBY, before get into suspend)&lt;/P&gt;&lt;P&gt;echo "mem" &amp;gt; /sys/power/state (getting into suspend)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo 1 &amp;gt; /sys/class/gpio/gpio204/value (in wakeup process)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the pop-click noise has gone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 08:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-SGTL5000-have-pop-noise-in-suspend-resume-and-shutdown/m-p/859115#M131209</guid>
      <dc:creator>bakbad</dc:creator>
      <dc:date>2019-01-31T08:05:06Z</dc:date>
    </item>
  </channel>
</rss>