<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX28  CHARGE_4P2_ILIMIT</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-CHARGE-4P2-ILIMIT/m-p/859081#M131202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get a problem when I'm charging a battery Lithium and runing the application , the current from the 5V is upper to the limit of the CHARGE_4P2_ILIMIT set.&lt;/P&gt;&lt;P&gt;I set to 400mA in CHARGE_4P2_ILIMIT and the current limit charge is set to 350mA.&lt;/P&gt;&lt;P&gt;I read on my power supply 434mA under 5V , and the current inside the batterys is 300mA.&lt;/P&gt;&lt;P&gt;I've nothing on the 5V power rail on my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why the current from the 5V power supply is more than the&amp;nbsp; limit of the CHARGE_4P2_ILIMIT&amp;nbsp; ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Feb 2019 15:30:34 GMT</pubDate>
    <dc:creator>david8</dc:creator>
    <dc:date>2019-02-13T15:30:34Z</dc:date>
    <item>
      <title>IMX28  CHARGE_4P2_ILIMIT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-CHARGE-4P2-ILIMIT/m-p/859081#M131202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get a problem when I'm charging a battery Lithium and runing the application , the current from the 5V is upper to the limit of the CHARGE_4P2_ILIMIT set.&lt;/P&gt;&lt;P&gt;I set to 400mA in CHARGE_4P2_ILIMIT and the current limit charge is set to 350mA.&lt;/P&gt;&lt;P&gt;I read on my power supply 434mA under 5V , and the current inside the batterys is 300mA.&lt;/P&gt;&lt;P&gt;I've nothing on the 5V power rail on my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why the current from the 5V power supply is more than the&amp;nbsp; limit of the CHARGE_4P2_ILIMIT&amp;nbsp; ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 15:30:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-CHARGE-4P2-ILIMIT/m-p/859081#M131202</guid>
      <dc:creator>david8</dc:creator>
      <dc:date>2019-02-13T15:30:34Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28  CHARGE_4P2_ILIMIT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-CHARGE-4P2-ILIMIT/m-p/859082#M131203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Laurent&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason may be that current from the 5V (VDD5V) provides power also for other linear regulators&lt;/P&gt;&lt;P&gt;as described on Figure 1. i.MX28 PMU AN4199 Using the i.MX28 Power Management Unit and Battery Charger&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4199.pdf" title="https://www.nxp.com/docs/en/application-note/AN4199.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4199.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 04:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-CHARGE-4P2-ILIMIT/m-p/859082#M131203</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-14T04:49:29Z</dc:date>
    </item>
  </channel>
</rss>