<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Need a package manager in Linux-imx</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858636#M131155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in the same position.&amp;nbsp; I bought this evaluation kit to evaluate if the hardware will work for our project.&amp;nbsp; I don't want to spend days or weeks doing a full Linux bring up just to install some standard packages like git, mongodb, nodejs, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You guys know this board, so you must be able to provide apt-get or yum or similar in&amp;nbsp;a Linux&amp;nbsp;image or give some instructions on how to build one of them from source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, are there no full Linux distribution images that will run on this board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Apr 2019 17:30:37 GMT</pubDate>
    <dc:creator>ken2</dc:creator>
    <dc:date>2019-04-11T17:30:37Z</dc:date>
    <item>
      <title>Need a package manager in Linux-imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858634#M131153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,there.&lt;/P&gt;&lt;P&gt;I'm using the imx8qxpmek board,and i want to install some software by a package manager (just like apt-get in Ubuntu and so on), is a tool like this available?&lt;/P&gt;&lt;P&gt;And I learned that there maybe a way to use the yocto, but when using yocto, it should flash the image once there is a modify, not convenience.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 09:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858634#M131153</guid>
      <dc:creator>chenchen_xi</dc:creator>
      <dc:date>2019-02-13T09:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: Need a package manager in Linux-imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858635#M131154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xi Chenchen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The i.MX BSP does not have a package manager like apt-get. You would need to add it to the Linux image. There is some information on the following documents, although further customization would be required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328199" target="test_blank"&gt;https://community.nxp.com/docs/DOC-328199&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/834043?commentID=834043#comment-834043"&gt;https://community.nxp.com/message/834043?commentID=834043#comment-834043&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope these help as a starting point!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 22:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858635#M131154</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-02-13T22:11:03Z</dc:date>
    </item>
    <item>
      <title>Re: Need a package manager in Linux-imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858636#M131155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in the same position.&amp;nbsp; I bought this evaluation kit to evaluate if the hardware will work for our project.&amp;nbsp; I don't want to spend days or weeks doing a full Linux bring up just to install some standard packages like git, mongodb, nodejs, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You guys know this board, so you must be able to provide apt-get or yum or similar in&amp;nbsp;a Linux&amp;nbsp;image or give some instructions on how to build one of them from source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, are there no full Linux distribution images that will run on this board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 17:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-a-package-manager-in-Linux-imx/m-p/858636#M131155</guid>
      <dc:creator>ken2</dc:creator>
      <dc:date>2019-04-11T17:30:37Z</dc:date>
    </item>
  </channel>
</rss>