<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN communication i.mx 53 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212872#M13088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Bests&lt;/P&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2012 12:23:44 GMT</pubDate>
    <dc:creator>Philippe</dc:creator>
    <dc:date>2012-02-28T12:23:44Z</dc:date>
    <item>
      <title>CAN communication i.mx 53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212867#M13083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been trying to use the CAN transceiver of the IMX53 board but I lack information on how to do it (I have read the pdf of the workshop). To be more specific I am looking for some kind of tutorial on how to set up CAN communication with the board, and also a pin diagram of CAN1 and CAN2 on the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance for your help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Philippe&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Purdue&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Feb 2012 01:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212867#M13083</guid>
      <dc:creator>Philippe</dc:creator>
      <dc:date>2012-02-18T01:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: CAN communication i.mx 53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212868#M13084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Was anybody able to use the CAN tools on the imx53 ARD board ? I deployed the canutils and libsocketcan packets, I then ran ./ltib, and finally I recreated the boot able sd card. But when I try to type canconfig or cansend on the linux console (running on the processor board), it says the command does not exist.&lt;/P&gt;&lt;P&gt;Please help, I've been stuck on this for the past week.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bests&lt;/P&gt;&lt;P&gt;Philippe Bongrain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Feb 2012 04:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212868#M13084</guid>
      <dc:creator>Philippe</dc:creator>
      <dc:date>2012-02-26T04:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: CAN communication i.mx 53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212869#M13085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check the to make sure that the Can utilities are installed on your SD card. On you SD card look under the folders /usr/bin/. There you should see the binary for the CAN utilities. If the binary is there make sure you are typing in the command in the terminal right. (i.e. canecho --help) If the CAN utilities are not there then you need to build the CAN utilities as shown on the .pdf from winter workshop. The spec files are located in ltib/dist/lfs-5.1/canutils. Note that this is in the same place as the the helloworld example, so you can use the same commands and process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the can pin outs, look at the schematic on the .pdf from winter workshop. The schematic shows what each pin is connected to.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alexander Keller&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 02:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212869#M13085</guid>
      <dc:creator>AlexanderKelle1</dc:creator>
      <dc:date>2012-02-27T02:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: CAN communication i.mx 53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212870#M13086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot for your help. I now have the can binaries in /usb/bin. I will just need to copy the new RFS to the SD card and I should be able to use CAN tools I hope.&lt;/P&gt;&lt;P&gt;I also recently faced a problem while using ltib: when running ./ltib I get this error:&lt;/P&gt;&lt;P&gt;Processing: fsl-mm-codeclib&lt;BR /&gt;=============================&lt;BR /&gt;Build path taken because: no prebuilt rpm, &lt;BR /&gt;Testing network connectivity&lt;BR /&gt;^Ckilled by SIGINT&lt;/P&gt;&lt;P&gt;Started: Mon Feb 27 07:53:56 2012&lt;BR /&gt;Ended: Mon Feb 27 07:54:19 2012&lt;BR /&gt;Elapsed: 23 seconds&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Build Failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am still trying to fix this so if you know what to do it would be very helpful!&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Philippe Bongrain&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;CITE&gt;Alexander Keller said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/can-communication-i-mx-53?groupUrl=ecocar2&amp;amp;#4103961Comment61364"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;Check the to make sure that the Can utilities are installed on your SD card. On you SD card look under the folders /usr/bin/. There you should see the binary for the CAN utilities. If the binary is there make sure you are typing in the command in the terminal right. (i.e. canecho --help) If the CAN utilities are not there then you need to build the CAN utilities as shown on the .pdf from winter workshop. The spec files are located in ltib/dist/lfs-5.1/canutils. Note that this is in the same place as the the helloworld example, so you can use the same commands and process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the can pin outs, look at the schematic on the .pdf from winter workshop. The schematic shows what each pin is connected to.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alexander Keller&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 12:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212870#M13086</guid>
      <dc:creator>Philippe</dc:creator>
      <dc:date>2012-02-27T12:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: CAN communication i.mx 53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212871#M13087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Philippe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-mm-codeclib can be downloaded on the Freescale web page.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53_SW"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look for multimedia codecs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, since you are not playing media, you don't need this package. I recommend you de-select it from the package list menu on LTIB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Renato&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2012 05:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212871#M13087</guid>
      <dc:creator>Frias</dc:creator>
      <dc:date>2012-02-28T05:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: CAN communication i.mx 53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212872#M13088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Bests&lt;/P&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2012 12:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-communication-i-mx-53/m-p/212872#M13088</guid>
      <dc:creator>Philippe</dc:creator>
      <dc:date>2012-02-28T12:23:44Z</dc:date>
    </item>
  </channel>
</rss>