<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to update the uboot &amp; kernel when linux is running in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-uboot-kernel-when-linux-is-running/m-p/855837#M130862</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ansen An,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This feature is not available on the i.MX BSP. However, you should be able to look for information about the Linux livepatch feature that I think satisfies your requirement. This feature allows to update the kernel without the need for reboot. You can find more information here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.kernel.org/doc/Documentation/livepatch/livepatch.txt"&gt;https://www.kernel.org/doc/Documentation/livepatch/livepatch.txt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Jan 2019 20:19:08 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-01-14T20:19:08Z</dc:date>
    <item>
      <title>How to update the uboot &amp; kernel when linux is running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-uboot-kernel-when-linux-is-running/m-p/855836#M130861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to update my linux under linux running.&lt;/P&gt;&lt;P&gt;Can somebody tell me how to do?&lt;/P&gt;&lt;P&gt;I.mx6ull+nand flash+ddr.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Jan 2019 08:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-uboot-kernel-when-linux-is-running/m-p/855836#M130861</guid>
      <dc:creator>alj79</dc:creator>
      <dc:date>2019-01-06T08:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to update the uboot &amp; kernel when linux is running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-uboot-kernel-when-linux-is-running/m-p/855837#M130862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ansen An,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This feature is not available on the i.MX BSP. However, you should be able to look for information about the Linux livepatch feature that I think satisfies your requirement. This feature allows to update the kernel without the need for reboot. You can find more information here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.kernel.org/doc/Documentation/livepatch/livepatch.txt"&gt;https://www.kernel.org/doc/Documentation/livepatch/livepatch.txt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 20:19:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-uboot-kernel-when-linux-is-running/m-p/855837#M130862</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-01-14T20:19:08Z</dc:date>
    </item>
  </channel>
</rss>