<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PWM API / PWM Library for IMX Linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855655#M130829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I am searching for libraries which can be used for PWM Operations especially with the stepper motors. I would like to interface with IMX Processors.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have searched on this community and on third party vendors, but i could not find any libraries which are focused on PWM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need any kind of Hardware with the stepper motor for implementing motors ? For example motor control chipset ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like some support from Community on this topic.&lt;/P&gt;&lt;P&gt;Thanks for Support and Help.&lt;/P&gt;&lt;P&gt;R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2019 12:30:26 GMT</pubDate>
    <dc:creator>rvalvekar</dc:creator>
    <dc:date>2019-02-12T12:30:26Z</dc:date>
    <item>
      <title>PWM API / PWM Library for IMX Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855655#M130829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I am searching for libraries which can be used for PWM Operations especially with the stepper motors. I would like to interface with IMX Processors.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have searched on this community and on third party vendors, but i could not find any libraries which are focused on PWM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need any kind of Hardware with the stepper motor for implementing motors ? For example motor control chipset ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like some support from Community on this topic.&lt;/P&gt;&lt;P&gt;Thanks for Support and Help.&lt;/P&gt;&lt;P&gt;R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 12:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855655#M130829</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-02-12T12:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: PWM API / PWM Library for IMX Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855656#M130830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rohan,&lt;/P&gt;&lt;P&gt;Linux BSP for i.MX processors include a basic PWM library (mainly oriented for LCD backlight control). Therefore, it is not intended to work with more real-time implementations like motor control and may not fit your timing requirements. Please refer to chapter 2.7 “Pulse-Width Modulator (PWM)” section of “i.MX Reference Manual” document (attached) for additional details.&lt;/P&gt;&lt;P&gt;In case of using a heterogeneous i.MX processor like the i.MX6SX, i.MX7 or i.MX8, you could use the included M4 core to control real-time applications, like motor control.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 19:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855656#M130830</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-02-12T19:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: PWM API / PWM Library for IMX Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855657#M130831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlos,&lt;/P&gt;&lt;P&gt;Thank you for the information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 08:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-API-PWM-Library-for-IMX-Linux/m-p/855657#M130831</guid>
      <dc:creator>rvalvekar</dc:creator>
      <dc:date>2019-02-26T08:39:46Z</dc:date>
    </item>
  </channel>
</rss>