<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Driving odd LED/LCD panel formats in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Driving-odd-LED-LCD-panel-formats/m-p/854970#M130761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking to drive odd panel formats with the i.MX8M - 1:1, 4:1 and 5.3:1 aspect ratios. Is there the capability to drive these formats and adjust the mipi output with a dumb LVDS converter (aka TI's SN65DSI84) to drive a panel directly or would I need an iumage converter like the Lattice SiliconImage series of devices?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Feb 2019 22:22:24 GMT</pubDate>
    <dc:creator>chrisrayner</dc:creator>
    <dc:date>2019-02-11T22:22:24Z</dc:date>
    <item>
      <title>Driving odd LED/LCD panel formats</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Driving-odd-LED-LCD-panel-formats/m-p/854970#M130761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking to drive odd panel formats with the i.MX8M - 1:1, 4:1 and 5.3:1 aspect ratios. Is there the capability to drive these formats and adjust the mipi output with a dumb LVDS converter (aka TI's SN65DSI84) to drive a panel directly or would I need an iumage converter like the Lattice SiliconImage series of devices?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Feb 2019 22:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Driving-odd-LED-LCD-panel-formats/m-p/854970#M130761</guid>
      <dc:creator>chrisrayner</dc:creator>
      <dc:date>2019-02-11T22:22:24Z</dc:date>
    </item>
    <item>
      <title>Re: Driving odd LED/LCD panel formats</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Driving-odd-LED-LCD-panel-formats/m-p/854971#M130762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at MIPI DSI panel driver for rm67191, which gives timing data without edid.&lt;/P&gt;&lt;P&gt;Adjust lcd timings in "struct display_timing rad_default_timing"&lt;BR /&gt;drivers\gpu\drm\panel\panel-raydium-rm67191.c&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-raydium-rm67191.c?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-raydium-rm67191.c?h=imx_4.14.78_1.0.0_ga"&gt;panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;sn65dsi85 example :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/482724"&gt;how to use ldb/lvds in android8 of imx8mq ?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;boundary devices lcd settings:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/yocto-release-for-i-mx8mq/" title="https://boundarydevices.com/yocto-release-for-i-mx8mq/"&gt;Yocto release for i.MX 8MQ - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 07:44:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Driving-odd-LED-LCD-panel-formats/m-p/854971#M130762</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-13T07:44:58Z</dc:date>
    </item>
  </channel>
</rss>