<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8M: Copy from eMMC to TCML</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Copy-from-eMMC-to-TCML/m-p/854550#M130703</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand from the documentation that Boot ROM initially loads 4K region starting from 0x8400 in eMMC to TCML and starts executing the code. I am writing a boot loader which exceeds 4K size.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any possibility that I can make Boot ROM copy remaining code?&lt;/P&gt;&lt;P&gt;Or should I include eMMC driver in the first 4K region and make it fetch remaining code for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bharat&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Feb 2019 20:52:22 GMT</pubDate>
    <dc:creator>bharatkumarbach</dc:creator>
    <dc:date>2019-02-11T20:52:22Z</dc:date>
    <item>
      <title>iMX8M: Copy from eMMC to TCML</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Copy-from-eMMC-to-TCML/m-p/854550#M130703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand from the documentation that Boot ROM initially loads 4K region starting from 0x8400 in eMMC to TCML and starts executing the code. I am writing a boot loader which exceeds 4K size.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any possibility that I can make Boot ROM copy remaining code?&lt;/P&gt;&lt;P&gt;Or should I include eMMC driver in the first 4K region and make it fetch remaining code for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bharat&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Feb 2019 20:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Copy-from-eMMC-to-TCML/m-p/854550#M130703</guid>
      <dc:creator>bharatkumarbach</dc:creator>
      <dc:date>2019-02-11T20:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M: Copy from eMMC to TCML</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Copy-from-eMMC-to-TCML/m-p/854551#M130704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bharat&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;boot ROM uses ivt for loading custom application as described in&lt;/P&gt;&lt;P&gt;Figure 6-18. Image Vector Table i.MX8MDQ Reference Manual &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;In general yes, recommended way is to implement eMMC custom&lt;/P&gt;&lt;P&gt;driver in small OCRAM region and make it fetch remaining code for custom application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 05:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Copy-from-eMMC-to-TCML/m-p/854551#M130704</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-12T05:37:09Z</dc:date>
    </item>
  </channel>
</rss>