<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel panic - not syncing: Attempted to kill init!</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853006#M130454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I meet a weird issue when porting linux 4.14.78. When the kernel try to start the init process,the kernel will enter a panic state.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CPU is imx28,and the cross compiler version is&amp;nbsp;Linaro GCC 7.3-2018.05.&lt;/P&gt;&lt;P&gt;The root file system is&amp;nbsp;busybox-1.29.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 3.661032] This architecture does not have kernel memory protection.&lt;BR /&gt;&lt;STRONG&gt;[ 3.721936] init (1): undefined instruction: pc=0007169e&lt;/STRONG&gt;&lt;BR /&gt;[ 3.727687] CPU: 0 PID: 1 Comm: init Not tainted 4.14.78-05578-g66620c3-dirty #7&lt;BR /&gt;[ 3.735402] Hardware name: Freescale MXS (Device Tree)&lt;BR /&gt;[ 3.740717] task: c7480000 task.stack: c7488000&lt;BR /&gt;[ 3.745528] PC is at 0x7169e&lt;BR /&gt;[ 3.748488] LR is at 0x225b7&lt;BR /&gt;[ 3.751434] pc : [&amp;lt;0007169e&amp;gt;] lr : [&amp;lt;000225b7&amp;gt;] psr: 40000030&lt;BR /&gt;[ 3.758039] sp : bea4ef0c ip : 00000000 fp : 00000000&lt;BR /&gt;[ 3.763629] r10: 00000000 r9 : 00000000 r8 : 00000000&lt;BR /&gt;[ 3.769023] r7 : 00000000 r6 : 00000000 r5 : 00000000 r4 : 00000000&lt;BR /&gt;[ 3.775886] r3 : 00000000 r2 : bea4ef14 r1 : 00000001 r0 : 00000000&lt;BR /&gt;[ 3.782581] Flags: nZcv IRQs on FIQs on Mode USER_32 ISA Thumb Segment user&lt;BR /&gt;[ 3.790256] Control: 0005317f Table: 46cdc000 DAC: 00000055&lt;BR /&gt;[ 3.796352] Code: 7803 4606 b913 2001 (e8bd) 83f8&lt;BR /&gt;[ 3.807013] Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004&lt;BR /&gt;[ 3.807013]&lt;BR /&gt;[ 3.816246] CPU: 0 PID: 1 Comm: init Not tainted 4.14.78-05578-g66620c3-dirty #7&lt;BR /&gt;[ 3.823695] Hardware name: Freescale MXS (Device Tree)&lt;BR /&gt;[ 3.828955] [&amp;lt;c00102d4&amp;gt;] (unwind_backtrace) from [&amp;lt;c000e0e4&amp;gt;] (show_stack+0x10/0x14)&lt;BR /&gt;[ 3.836806] [&amp;lt;c000e0e4&amp;gt;] (show_stack) from [&amp;lt;c0019b68&amp;gt;] (panic+0xbc/0x23c)&lt;BR /&gt;[ 3.843768] [&amp;lt;c0019b68&amp;gt;] (panic) from [&amp;lt;c001c490&amp;gt;] (do_exit+0xa1c/0xa68)&lt;BR /&gt;[ 3.850546] [&amp;lt;c001c490&amp;gt;] (do_exit) from [&amp;lt;c001d6c4&amp;gt;] (do_group_exit+0x38/0xbc)&lt;BR /&gt;[ 3.857866] [&amp;lt;c001d6c4&amp;gt;] (do_group_exit) from [&amp;lt;c0028690&amp;gt;] (get_signal+0x20c/0x818)&lt;BR /&gt;[ 3.865610] [&amp;lt;c0028690&amp;gt;] (get_signal) from [&amp;lt;c000d3a4&amp;gt;] (do_signal+0xc4/0x448)&lt;BR /&gt;[ 3.872913] [&amp;lt;c000d3a4&amp;gt;] (do_signal) from [&amp;lt;c000d900&amp;gt;] (do_work_pending+0xc8/0xe8)&lt;BR /&gt;[ 3.880564] [&amp;lt;c000d900&amp;gt;] (do_work_pending) from [&amp;lt;c000a7b4&amp;gt;] (slow_work_pending+0xc/0x20)&lt;BR /&gt;[ 3.888852] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the busybox binary objdump:&lt;/P&gt;&lt;P&gt;7195c: 23004a94 movwcs r4, #2708 ; 0xa94&lt;BR /&gt; 71960: 41f0e92d mvnsmi lr, sp, lsr #18&lt;BR /&gt; 71964: 9308b08c movwls fp, #32908 ; 0x808c&lt;BR /&gt; 71968: e9cd460e stmib sp, {r1, r2, r3, r9, sl, lr}^&lt;BR /&gt; 7196c: 930b2309 movwls r2, #45833 ; 0xb309&lt;BR /&gt; 71970: fcdcf003 ldc2l 0, cr15, [ip], {3}&lt;BR /&gt; 71974: 46042307 strmi r2, [r4], -r7, lsl #6&lt;BR /&gt; 71978: f7a06003 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xf7a06003&lt;BR /&gt; 7197c: b118fd11 tstlt r8, r1, lsl sp ; &amp;lt;UNPREDICTABLE&amp;gt;&lt;BR /&gt; 71980: f0436823 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xf0436823&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone can give some advices for it?&lt;/P&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 05 Jan 2019 11:04:44 GMT</pubDate>
    <dc:creator>liuxing</dc:creator>
    <dc:date>2019-01-05T11:04:44Z</dc:date>
    <item>
      <title>Kernel panic - not syncing: Attempted to kill init!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853006#M130454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I meet a weird issue when porting linux 4.14.78. When the kernel try to start the init process,the kernel will enter a panic state.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CPU is imx28,and the cross compiler version is&amp;nbsp;Linaro GCC 7.3-2018.05.&lt;/P&gt;&lt;P&gt;The root file system is&amp;nbsp;busybox-1.29.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 3.661032] This architecture does not have kernel memory protection.&lt;BR /&gt;&lt;STRONG&gt;[ 3.721936] init (1): undefined instruction: pc=0007169e&lt;/STRONG&gt;&lt;BR /&gt;[ 3.727687] CPU: 0 PID: 1 Comm: init Not tainted 4.14.78-05578-g66620c3-dirty #7&lt;BR /&gt;[ 3.735402] Hardware name: Freescale MXS (Device Tree)&lt;BR /&gt;[ 3.740717] task: c7480000 task.stack: c7488000&lt;BR /&gt;[ 3.745528] PC is at 0x7169e&lt;BR /&gt;[ 3.748488] LR is at 0x225b7&lt;BR /&gt;[ 3.751434] pc : [&amp;lt;0007169e&amp;gt;] lr : [&amp;lt;000225b7&amp;gt;] psr: 40000030&lt;BR /&gt;[ 3.758039] sp : bea4ef0c ip : 00000000 fp : 00000000&lt;BR /&gt;[ 3.763629] r10: 00000000 r9 : 00000000 r8 : 00000000&lt;BR /&gt;[ 3.769023] r7 : 00000000 r6 : 00000000 r5 : 00000000 r4 : 00000000&lt;BR /&gt;[ 3.775886] r3 : 00000000 r2 : bea4ef14 r1 : 00000001 r0 : 00000000&lt;BR /&gt;[ 3.782581] Flags: nZcv IRQs on FIQs on Mode USER_32 ISA Thumb Segment user&lt;BR /&gt;[ 3.790256] Control: 0005317f Table: 46cdc000 DAC: 00000055&lt;BR /&gt;[ 3.796352] Code: 7803 4606 b913 2001 (e8bd) 83f8&lt;BR /&gt;[ 3.807013] Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004&lt;BR /&gt;[ 3.807013]&lt;BR /&gt;[ 3.816246] CPU: 0 PID: 1 Comm: init Not tainted 4.14.78-05578-g66620c3-dirty #7&lt;BR /&gt;[ 3.823695] Hardware name: Freescale MXS (Device Tree)&lt;BR /&gt;[ 3.828955] [&amp;lt;c00102d4&amp;gt;] (unwind_backtrace) from [&amp;lt;c000e0e4&amp;gt;] (show_stack+0x10/0x14)&lt;BR /&gt;[ 3.836806] [&amp;lt;c000e0e4&amp;gt;] (show_stack) from [&amp;lt;c0019b68&amp;gt;] (panic+0xbc/0x23c)&lt;BR /&gt;[ 3.843768] [&amp;lt;c0019b68&amp;gt;] (panic) from [&amp;lt;c001c490&amp;gt;] (do_exit+0xa1c/0xa68)&lt;BR /&gt;[ 3.850546] [&amp;lt;c001c490&amp;gt;] (do_exit) from [&amp;lt;c001d6c4&amp;gt;] (do_group_exit+0x38/0xbc)&lt;BR /&gt;[ 3.857866] [&amp;lt;c001d6c4&amp;gt;] (do_group_exit) from [&amp;lt;c0028690&amp;gt;] (get_signal+0x20c/0x818)&lt;BR /&gt;[ 3.865610] [&amp;lt;c0028690&amp;gt;] (get_signal) from [&amp;lt;c000d3a4&amp;gt;] (do_signal+0xc4/0x448)&lt;BR /&gt;[ 3.872913] [&amp;lt;c000d3a4&amp;gt;] (do_signal) from [&amp;lt;c000d900&amp;gt;] (do_work_pending+0xc8/0xe8)&lt;BR /&gt;[ 3.880564] [&amp;lt;c000d900&amp;gt;] (do_work_pending) from [&amp;lt;c000a7b4&amp;gt;] (slow_work_pending+0xc/0x20)&lt;BR /&gt;[ 3.888852] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the busybox binary objdump:&lt;/P&gt;&lt;P&gt;7195c: 23004a94 movwcs r4, #2708 ; 0xa94&lt;BR /&gt; 71960: 41f0e92d mvnsmi lr, sp, lsr #18&lt;BR /&gt; 71964: 9308b08c movwls fp, #32908 ; 0x808c&lt;BR /&gt; 71968: e9cd460e stmib sp, {r1, r2, r3, r9, sl, lr}^&lt;BR /&gt; 7196c: 930b2309 movwls r2, #45833 ; 0xb309&lt;BR /&gt; 71970: fcdcf003 ldc2l 0, cr15, [ip], {3}&lt;BR /&gt; 71974: 46042307 strmi r2, [r4], -r7, lsl #6&lt;BR /&gt; 71978: f7a06003 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xf7a06003&lt;BR /&gt; 7197c: b118fd11 tstlt r8, r1, lsl sp ; &amp;lt;UNPREDICTABLE&amp;gt;&lt;BR /&gt; 71980: f0436823 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xf0436823&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone can give some advices for it?&lt;/P&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Jan 2019 11:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853006#M130454</guid>
      <dc:creator>liuxing</dc:creator>
      <dc:date>2019-01-05T11:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic - not syncing: Attempted to kill init!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853007#M130455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;sorry,&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;the busybox binary objdump&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;71688: 43f8e92d mvnsmi lr, #737280 ; 0xb4000&lt;BR /&gt; 7168c: 460c4607 strmi r4, [ip], -r7, lsl #12&lt;BR /&gt; 71690: f0034615 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xf0034615&lt;BR /&gt; 71694: 7803ffd1 stmdavc r3, {r0, r4, r6, r7, r8, r9, sl, fp, ip, sp, lr, pc}&lt;BR /&gt; 71698: b9134606 ldmdblt r3, {r1, r2, r9, sl, lr}&lt;BR /&gt; 7169c: e8bd2001 pop {r0, sp}&lt;BR /&gt; 716a0: 692383f8 stmdbvs r3!, {r3, r4, r5, r6, r7, r8, r9, pc}&lt;BR /&gt; 716a4: 4370f403 cmnmi r0, #50331648 ; 0x3000000 ; &amp;lt;UNPREDICTABLE&amp;gt;&lt;BR /&gt; 716a8: 4f40f5b3 svcmi 0x0040f5b3&lt;BR /&gt; 716ac: 4857d104 ldmdami r7, {r2, r8, ip, lr, pc}^&lt;BR /&gt; 716b0: f09f4639 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xf09f4639&lt;BR /&gt; 716b4: e7f1f930 ; &amp;lt;UNDEFINED&amp;gt; instruction: 0xe7f1f930&lt;BR /&gt; 716b8: 4f80f5b3 svcmi 0x0080f5b3&lt;BR /&gt; 716bc: 0200f04f andeq pc, r0, #79 ; 0x4f&lt;BR /&gt; 716c0: d01c612a andsle r6, ip, sl, lsr #2&lt;BR /&gt; 716c4: 2b016963 blcs 0xcbc58&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Jan 2019 02:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853007#M130455</guid>
      <dc:creator>liuxing</dc:creator>
      <dc:date>2019-01-06T02:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic - not syncing: Attempted to kill init!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853008#M130456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi xing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ususally kernel panic is caused by memory errors so one can recheck it&lt;/P&gt;&lt;P&gt;with memory test&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1455"&gt;Board Bring-up and DDR Initialization Tools&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Jan 2019 22:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-not-syncing-Attempted-to-kill-init/m-p/853008#M130456</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-06T22:55:58Z</dc:date>
    </item>
  </channel>
</rss>