<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PD/PU resistor values on GPIO of i.MX8M in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852215#M130377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In IMX8MDQLQIEC, there are two different number for PD/PU resistor values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table 26&amp;nbsp; says,&lt;/P&gt;&lt;P&gt;30 x 0.75 Kohms (min) , 30 Kohms(typ),&amp;nbsp; 30 x 1.25 Kohms(max.) for PU.&lt;/P&gt;&lt;P&gt;95 x 0.75&amp;nbsp;&lt;SPAN&gt;Kohms (min) ,&amp;nbsp;&lt;/SPAN&gt; 95Kohms(typ),&amp;nbsp; 95 x 1.25 Kohms(max) for PD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table 84 says&lt;/P&gt;&lt;P&gt;90 Kohms(PD)&lt;/P&gt;&lt;P&gt;27 Kohms(PU)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;** It says GPIO1_IO02 has 27Kohms PD. It seems to be typo.&lt;/P&gt;&lt;P&gt;If the table 84 refers to typ value in Table 26, it make sense.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that PU/PD on silicon are not so accurate, so these small difference doesn't matter for NXP.&lt;/P&gt;&lt;P&gt;But the values should be the same and consistent to avoid confusion at your&amp;nbsp; customer's site.&lt;/P&gt;&lt;P&gt;Can we take PD/PU resistor value in Table 26 as your authorized value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Norihiro Michigami&lt;/P&gt;&lt;P&gt;AVNET&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Mar 2019 10:08:13 GMT</pubDate>
    <dc:creator>Norihiro</dc:creator>
    <dc:date>2019-03-26T10:08:13Z</dc:date>
    <item>
      <title>PD/PU resistor values on GPIO of i.MX8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852215#M130377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In IMX8MDQLQIEC, there are two different number for PD/PU resistor values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table 26&amp;nbsp; says,&lt;/P&gt;&lt;P&gt;30 x 0.75 Kohms (min) , 30 Kohms(typ),&amp;nbsp; 30 x 1.25 Kohms(max.) for PU.&lt;/P&gt;&lt;P&gt;95 x 0.75&amp;nbsp;&lt;SPAN&gt;Kohms (min) ,&amp;nbsp;&lt;/SPAN&gt; 95Kohms(typ),&amp;nbsp; 95 x 1.25 Kohms(max) for PD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table 84 says&lt;/P&gt;&lt;P&gt;90 Kohms(PD)&lt;/P&gt;&lt;P&gt;27 Kohms(PU)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;** It says GPIO1_IO02 has 27Kohms PD. It seems to be typo.&lt;/P&gt;&lt;P&gt;If the table 84 refers to typ value in Table 26, it make sense.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that PU/PD on silicon are not so accurate, so these small difference doesn't matter for NXP.&lt;/P&gt;&lt;P&gt;But the values should be the same and consistent to avoid confusion at your&amp;nbsp; customer's site.&lt;/P&gt;&lt;P&gt;Can we take PD/PU resistor value in Table 26 as your authorized value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Norihiro Michigami&lt;/P&gt;&lt;P&gt;AVNET&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 10:08:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852215#M130377</guid>
      <dc:creator>Norihiro</dc:creator>
      <dc:date>2019-03-26T10:08:13Z</dc:date>
    </item>
    <item>
      <title>Re: PD/PU resistor values on GPIO of i.MX8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852216#M130378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&amp;nbsp; The Datasheet table &lt;SPAN class=""&gt;26 (GPIO DC parameters) is correct regarding pull-up resistor 30K +/- 0.25K &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;and pull-down resistor 95K +/- 0.25K.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; As for the GPIO1_IO02: customers can use IOMUXC registers, in particular -&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;IOMUXC_SW_PAD_CTL_PAD_GPIO1_IO02 - to define what pins have internal 27K Ohm &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;pull up resistor enabled. &lt;/SPAN&gt;The bit PUE of&amp;nbsp;&lt;SPAN class=""&gt;IOMUXC_SW_PAD_CTL_PAD_GPIO1_IO02&lt;/SPAN&gt; is set. &lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&amp;nbsp; Note, &lt;SPAN class=""&gt;i.MX8M GPIOs have internal PD(90K), which can’t be disabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2019 04:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852216#M130378</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-03-27T04:20:55Z</dc:date>
    </item>
    <item>
      <title>Re: PD/PU resistor values on GPIO of i.MX8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852217#M130379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I understood that default value of PUE bit for IOMUXC_SW_PAD_CTL_PAD_GPIO1_IO02 is enabled whereas&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;PUE for other GPIO is disabled basically.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Norihiro Michigami&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;AVNET&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 04:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PD-PU-resistor-values-on-GPIO-of-i-MX8M/m-p/852217#M130379</guid>
      <dc:creator>Norihiro</dc:creator>
      <dc:date>2019-03-28T04:56:05Z</dc:date>
    </item>
  </channel>
</rss>